Part Number: TL16C754C Dear Team,
Currently, the customer is using CP2108 for USB to UART 4 output application.
I find TL16C754C , but not sure this one is suitable here or not.
Can you check on which one is suitable to compare with CP2108 ?
It will be…
Part Number: TL16C754C Other Parts Discussed in Thread: TL16C554A Hi team,
It is nice to know you here. My customer is evaluating TL16C754C. And they met below issue,
The TX data can be received by PC;
When PC sending data to this device, such as "11…
Part Number: TL16C754C Hi all,
Does the TL16CP754C can be safely interfaced with an 5V powered RS485 transceiver when it is powered under 3.3V.
As this this chip can be powered from 1.8v, 3v3, or 5v, I just would like to know if it's 5V tolerant on the…
Part Number: TL16C754C Hello TI,
I am using a TL16CP754CI part in my design for RS485 communciation.
The observation is that the part which is on board i.e., " 84AG1DN – TL16CP754CI" is highly sensitive to the temperature change caused by radiated…
Part Number: TL16C754C Does the TL16CP754C eliminate the stop-bit issue in the TL16C754C described here?:
http://www.ti.com/lit/er/sllz058a/sllz058a.pdf
If not, what is the suggested pin-compatible replacement for the TL16C754C?
Thanks!
-David
Part Number: TL16C754C Other Parts Discussed in Thread: MAX3243 , TM4C1294KCPDT , TL16C554A Hi,
I am using the TL16C754CPM device, where its Channels A & B are going out to a DB9 connector (through a MAX3243), Channels C & D are going to two UART channels…
Part Number: TL16C754C Hi,
1.System: Wince
2.TL16CP754CI sent & receive data is right when my data is less than 20byte.
3.If my data is long than 20byte TL16CP754 will return
SERIAL_IIR_RLS interrupt successive, It means RX_FIFO error.
Now read…
Part Number: TL16C754C Hi,
What is the difference between TL16 CP 754C and TL16 C 754C?
www.ti.com/.../tl16c754c.pdf
Where is the description of the difference in the data sheet?
Best regards, Seishin