Part Number: TL1963A-Q1 Hi team,
my customer is seeking the 12V to 5V/2A version LDO, is there any recommendation?
please let us know if there are any suggestions, automotive version is not a MUST.
Best regards
Fanbin
Part Number: TL1963A Hi,
Regarding 1.8V LDO TL1963A-18DCQR, can you please let me know Peak output current value ?
Application: 1.8V LDO to be used as Auxiliary supply for FPGA Spartan 7.
Regards,
Puspam
Part Number: TL1963A-Q1
Hi support team, Why are the RθJA of TL1963AQKTTRQ1 and TL1963AKTTR different?
TL1963AQKTTRQ1 RθJA=22.8℃/W TL1963AKTTR RθJA=32.9℃/W
Regards, Dice-K
Part Number: TL1963A Hi,
*1. According to the TL1963A datasheet P.16 "Chapter 10.1.1 ", output capacitor is min 10uF with <=3 ohm ESR to prevent oscillations. Is "this 10uF" value after de-rating or not? Please advise us.
*2. Is it…
Part Number: TL1963A-Q1 Hi Team, Do we have information on the maximum dimensions of the TL1963AQKTTRQ1 thermal pad? Unfortunately only the minimum dimensions were specified (Highlighted below). Thanks in advance! Kind Regards, Jejomar
Part Number: TL1963A Hello All ,
We are planning to use TL1963A-33KTTR to replace existing LDO as shown below .
If i place TL1963-33 directly on existing layout with 'SENSE' pin connected to 470pf capacitor as shown below .
Datasheet says ,…
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TLV767-Q1 Hi team,
We have design in TL1963-Q1 replacing OnSemi NCV57152DSADJR4G. From datasheet description, the operation temperature range is up to 125C. However, in the abs max rating table the…
Part Number: TL1963A-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have LDO that can support following spec?
SPE :
1.Vin=16V
2.Vo=8V
3.Io_max=1A
4.IC temperature is less than 100 degrees when Io_max
>>> TL1963A-Q1…
Part Number: TL1963A Hi,
Good Day. I have a customer who is working with TL1963A. Please see below his query for your reference. Thank you very much.
Datasheet on TL1963A-33. On page 6 in the Electrical Characteristics table, the Load Regulation states…