Part Number: TL1963A-Q1 Hello ,
I am looking for a confirmation regading the process FAB Technology of the TL1963A-Q1 , It is entirely BIPOLAR fom the input, through the signal path, to the output The emitter area ? Or a CMOS transistors variant that…
Part Number: TL1963A Other Parts Discussed in Thread: TPS7A26 Hi Team,
My customer is using Vin = 16V,Vout = 15V.
I found a “Quiescent current in shutdown” in the datasheet.
This operating condition is Vin = 6V. However I would like to know…
Hi Manoj,
Can you use one of these regulators instead? These will allow your inputs to go negative (well beyond -6.5V) without exceeding the abs max ratings of the device.
TPS73801 TL1963A-Q1
Here are some additional options from TI.com (hopefully that…
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TL1963A Dears,
I use TL1963A-Q1 to convert 13.5V input voltage to 12V output voltage, with the ShutDown pin of TL1963A-Q1 being controlled by external controller. Please see the schematics below…
Part Number: TL1963A-Q1 Hello ,
I am looking for some informations regading the process FAB Technology of the TL1963A-Q1 :
-The Mask SET / The die Revision .
-How we can get easily the FAB Site / The Diffusion Lot /the Wafer N°
Those requested datas…
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TPS7B70-Q1 , TPS7A60-Q1 Hello.
My customer requested to share the CTE information of ICs below.
CTE (Coefficient of Thermal Expansion) of TL1963ADCQR(Lead Frame) .
CTE (Coefficient of Thermal Expansion…
Part Number: TL1963A-Q1
Hi,
I have used LDO P/N TL1963AQKTTRQ1 in one of my design for 5V to 1.8V step down.
Design details:
Vin: 4.5V to 5.5V
Vout (expected): 1.8V @500mA
ADJ pin resistors: R2: 1.96k Ohms, R1: 4.02k Ohms
While probing the Vout, I observed…
Part Number: TL1963A In the datasheet, on Page 7, the table says ADJ pin bias current is typically 3uA at 25C, but on page 11, in Figure 19, the curve shows that Iadj is around 1.75uA at 25C. On page 17, the design example uses 3uA. It will probably only…