Part Number: TL2575HV-05-Q1 Hi,
I have to use this part TL2575HV-05QKTTRQ1 in circuit. But before finalize this part we need confirmation on it's grade, whether it is automotive grade or not?
There is no information mentioned in it's datasheet. But…
Part Number: TL2575HV-05-Q1 Hi dears
I was looking for a switching voltage regulator with low switching frequency. So I found the TL2575HV-05QKTTRQ1 on mouser website.
When I try to found some layout guidelines on the datasheet. I realized it is missing…
Part Number: TL2575HV-05-Q1 We're using the TL2575HV-05-Q1 to drop a 48V input to 5V to feed some LEDs, and then an LDO to 3.3V which feeds a PIC with PWM. Total current draw at the 5V load is less than 1A.
Schematic:
C3 = EEV-FK1K101Q , 80V rating…
Part Number: TL2575HV-05-Q1 The datasheet for the TL2575HV-05Q1 says that the ON/OFF pin can be safely tied to Vin, but then specifies TTL/CMOS as its input. There is no maximum voltage called out in the absolute maximum ratings section. If we want to…
Part Number: TL2575HV-05-Q1 I want to know efficiency calculation for this part number TL2575HV-05-Q1 with formula.
Vin = 54v and Iload = 500mA
Please reply me as soon as possibile.
Part Number: TL2575HV-05 Hi team, We received PCN. PCN said Package Outline Difference. In that comment, it says that shift component placement by 1.8mm towards the lead solder pad. Looking at the board layout, I think it can be implemented without shifting…
Other Parts Discussed in Thread: TL2575HV-05 Hi everybody,
I need to do this schematic for my board:
It's possible to have square waveform at my input Vin (0 to 24V). I have any others solutions for supplie my DC/DC regulator. So my question is…
Part Number: TL2575HV-05 Dear specialists,
My customer is designing TL2575HV-05.
He is thinking original circuit, I would be grateful if you could advise.
---
I'd like to know the accuracy and absolute value of the feedback resistor.
The background…