Part Number: TL2575HV-15 I have connected TL2575HV-15 as a buck converter. It supplies two POL regulators: a buck converter and a buck-boost converter, which are realized using LM2576-05 IC. The diodes connected are Schottky Diodes. The values of the…
Other Parts Discussed in Thread: TL2575HV-05 Hi everybody,
I need to do this schematic for my board:
It's possible to have square waveform at my input Vin (0 to 24V). I have any others solutions for supplie my DC/DC regulator. So my question is : what…
Hi,
Thank You for using E2E. The TPS65219 20W -Q1 is a pre-programmed device that comes with the default register settings to power the Sitara AM62x-Q1 processor and other processor with similar power/sequence requirements. The following Technical Reference…
Hi Glenn,
Since this problem is a customer after-sales problem for the time being, we can only get a set of data and the problem time log to print screenshots of several register values such as 0X4D, 0X4E (in the attachment). FPD LINK is connected to…
Hi Yazhi,
I would recommend selecting Butterworth 2 in the TIBQ tool, this helps by providing 2nd order filter coefficients, I think the reason your code didn't work is because it's missing the N2 and D2 coefficients.
I used the below code:
# I2C…
Part Number: BQ79612-Q1 Hello everyone,
We are currently developing an accumulator management system based on the BQ79612-Q1. Our first approach is to build a master module consisting of our microcontroller (STM32G474) and one BQ79612 as a base device…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH Hi Ti expert
I have some questions about system exceptions.
Hardware platform: TDA4VH
Software Version : SDK 8.6
Our custome board has two TDA4VHs, both of which are enabled with CPSW2G…
Part Number: DS90UB941AS-Q1 Hi,
HW: DS90UB941
Platform: NXP I.MX8MP
Our DS90UB941 (connected with DS90UB948) has a problem.
When Kernel init FPD-LINK driver, if it was on built-in driver , 3 piece of our DS90UB941 got i2c R/W error to DS90UB948(NAK) . …
Hello Kadeem,
Thank you very much for your support.
I got their data generated by Ver 1.7.6.2. and I attached it. (I changed extension from .hxt to .txt because the .hxt file can not be attached to this thread. So please change the file extension back to…
Part Number: TPS7B69 Dear Technical Support, Good day!
The parts that will be purchased by NIKKO CORPORATION is for automotive use.
And require IMDS registration for the supplier of the parts. Does TI have IMDS registration ?
Please help verify.
…