Part Number: TL3472 Other Parts Discussed in Thread: TEST Hi team,
When my customer use TL3472 for over current protection, they found at high current the drift of amps is too much and reaches the OCP limit, while during lab test, they only do fuction…
Part Number: TL3472 Dear All,
I'm using the TL3472 to drive the excitation signal for a resolver. I would like to know if there are VOL and VOH vs IOUT values available for the TL3472 ?
Application conditions :
- power supply : +12V / 0V
- peak current…
Part Number: TL3472 Hi there,
can you please confirm that the TLE3472 is able to handle in total up to 36V for (Vcc+ - Vcc-).
So e.g. up to Vcc- = -10V and Vcc+ = +26V should be fine even if the Datasheet absolute maximum ratings says Vcc+ = 18V. (Of course…
Part Number: TL3472 Dear all:
We have used TL3472 op amp to make frequency converter products. At present, it is found that 5 boards are damaged when TL3472 is powered on.The circuit diagram is as follows.
Under normal circumstances, when S1 is 0V,…
Part Number: TL3472 Other Parts Discussed in Thread: TINA-TI , , TEST Tool/software: TINA-TI or Spice Models Dear all,
This Robin Liu, FAE from S TL3472.TSC henzhen. Now our customer use TL347x as single supply op-amp to amplifier the 0~200mV voltage input…
Hello Li,
That is the bottom look at the top.
A similar post here (bottom markings) ; https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1066607/tl3472-bottom-side-part-marking-question-tl3472id-r
Part Number: TL3472-Q1 Other Parts Discussed in Thread: LM2904 , Hello Team,
As same case as the thread below “LM2904 crossover distortion happens”, my customer is evaluating LM2904 and struggled by cross-over distortion.
https://e2e.ti.com…
Part Number: TL3472-Q1 Other Parts Discussed in Thread: TL082-Q1 Hello,
Could you please let me know the slew rate variation of the following conditions? 1. Slew rate vs. Vcc+=10V to 16V, Vcc-=0V 2. Slew rate vs. temperature (Ta=-40C to +125C)
Best Regards…