Part Number: TL4242-Q1 Hi team,
Customer need to evaluate which thermal performance is better between TL4242QKTTRQ1 and Infineon TLE4242G ,
Do you have the thermal resistance comparison between TL4242QKTTRQ1 and Infineon TLE4242G? Or any comment for this? …
Part Number: TL4242-Q1 The datasheet says the current setting equation applies between 0.39 and 10R, but doesn't specify a minimum output current. I would like to use this part to run a string of LEDs at 35mA, which requires a 22R reference resistor …
Part Number: TL4242-Q1 Is the behaviour of the part predicatble with PWM input voltages between the maximum low and minimum high voltages? I would like a simple, low-cost method for shutting off the light when the temperature hits a maximum specified…
Part Number: TL4242-Q1 Other Parts Discussed in Thread: TPS92610-Q1 , , TL4242 Actually i need spice model for TL4242-Q1 and TPS92610-Q1. I am using Micro Cap 11 Simulation Tool.
I try to contact via your site but i can't. Finally i get this route - contact…
Part Number: TL4242-Q1 Are there any STEP files available for the above part in the WSON package? I've tried my usual sources for such things, but can't find it under the part number or the package name.
Part Number: TL4242 Hi team
TL4242-Q1 is in use.
I do not understand the block diagram in the datasheet.
Is it possible to describe as much as possible?
Thanks,
TM
Part Number: TL4242-Q1 Other Parts Discussed in Thread: LM3402 , TL4242 Hi there,
Since TL4242-Q1 is a current-controlled regulator, I'm wondering how the output voltage is determined?
In another current-controlled device LM3402, I found a description…
Part Number: TL4242
1. I have to connect a 3W white led light as here: http://tinyurl.com/jpj3gnu & control its intensity using a 10K potentiometer.
2. If = 0.7A Vf min = 3.2V Vf max = 4.0V
Input voltage range: 5.4V to 8.4V . Max current we can limit…