Part Number: TL4242 dear Sir
TL4242 can't be used in our project ,due the package size is big
1. We would like to find 3x3mm solution without choke
2. Led current could be modify by resistor
3. Iout small than 50mA
4. linear structure but…
Part Number: TL4242-Q1 Are there any STEP files available for the above part in the WSON package? I've tried my usual sources for such things, but can't find it under the part number or the package name.
Part Number: TL4242-Q1 Is the behaviour of the part predicatble with PWM input voltages between the maximum low and minimum high voltages? I would like a simple, low-cost method for shutting off the light when the temperature hits a maximum specified…
Part Number: TL4242TL4242 is a constant current LED driver IC. I am confused by the "Constant Current".
If there is a PWM input at Pin1, then the output Pin6 is PWM? If there is a shunt resistor at Pin 4, this pin is also PWM? How does TL4242 control…
All the model we have can be found on ti.com. there is already model for TPS92610-Q1 and TL4242 on ti.com
www.ti.com/.../toolssoftware
www.ti.com/.../toolssoftware
www.ti.com/.../toolssoftware
Other Parts Discussed in Thread: TL4242 , TPS22910A Hello.
My customer is currently in using TL4242,now.
I have gotten a question about this product .
So, please teach me about TL4242.
<Question>
Is there a method to keep the 10usec(max) in…
Other Parts Discussed in Thread: TL4242 Dear Sir
Below is MIC4802’s Dimming SPEC 200Hz~500KHz ,How about TL4242??
Does TI have any Duty vs LED current curve ??
Thanks
Other Parts Discussed in Thread: TL4242 Hi all Would you mind if we ask TL4242? How much is the maximum PWM frequnecy? Is it 1/Delay time turn on/off = 25kHz? Kind regards, Hirotaka Matsumoto