Other Parts Discussed in Thread: TL4242 I'm working on a design using the TL4242 to drive a string of LEDs via a 12" cable. The IC and the RREF resistor will be local but the LEDs will be across the cable.
My questions:
Should I build in any…
Other Parts Discussed in Thread: TL4242 Hello,
We've bought the TL4242 evaluation board to test with Wurth power leds ( datasheet - code 158353027) . Vf is 3.2V, If is 350mA, (can handle max 1A)
Testing the board with 6 leds in series mounted on a heat…
Other Parts Discussed in Thread: TPS92630-Q1 , TL4242-Q1 , TPS92638-Q1 Hello, Could you please let me know the minnimum regulation current of TPS92630-Q1 / TL4242-Q1 ? I understood that this device outoput current(min) is 10mA/ch. However our customer request…
Other Parts Discussed in Thread: TL4242 Hello,
How to use the TL4242 for low LED current (<10 ma)?
The equation given in the datasheet (I=0.177V/Rext) is good only for Rext up to 10 ohms?
What is the equation for higher value of Rext?
What is the relationship…
Other Parts Discussed in Thread: TL4242 , TL4242-Q1 Could you help to answer an urgent case!
Can you advice the thermal resistance of Junction to Case for TL4242? Customer would like to calculate accurate die temperature based on this parameter.
TL4242…
Other Parts Discussed in Thread: TL4242-Q1 Hello, Our customer evaluate TL4242-Q1 by the following conditions. Could you please let me know recommended pcb rayout or example ? --- Vin:9V to 16V Iout:450mA Vf(max) : 3V LED : 2series --- In this condition, Power…
Other Parts Discussed in Thread: TL4242 Hi,
I have one question about TL4242.
In case of connecting Rrff=0.95 ohm, the constant current will be 200mA. If it occurs output short on this condition, how much flow the current?
Thanks in advance.
Hide
Other Parts Discussed in Thread: TL4242-Q1 , TL4242 , TPS92630-Q1 Hello,
I have the question about TL4242-Q1.
Please see the attached file as our application and question.
4667.20140217_TL4242 operation.pdf
I would like to know the LED open detect functions…