Part Number: TL431-Q1 Tool/software: Hello Team,
I am looking for the voltage reference IC. Which is having below specification:
Vin= 12V to 24V
Vout = 0.5V to 0.8V
tolerance= 0.1% to 1%
Qualification= Automotive qualified AEC-Q1
current…
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431 , TLA431 Tool/software: Hi Teams,
The customer built a circuit according to the application circuit in the TL431 manual, as shown in the following figure,
They want to confirm three questions…
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431 , TPS3762-Q1 Tool/software: Hello Team,
We are looking for an IC for undervoltage and overvoltage protection which is having below specifications:
Vin= 36V to 65V
tolerance = TBD
Qualification…
Part Number: TL431-Q1 Tool/software: Hi,
Plesae advise if TI can provide the IMDS file for the auto-grade device, like the TL431AQDBZRQ1 and so on, thanks.
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431 Tool/software: Is it possible to use the TL431-Q1 shunt regulator as a supercapacitor balancer?
I have a 12V supply with the output current limited to 100mA . If I understand this correctly…
Part Number: TL431-Q1 Hi team,
My customer is testing TL431-Q1 and captured below sawtooth shape Vka waveform, could you help suggest why it happens?
Customer is testing with below circuit, input resistor 2.15k, R1 10K R2 21.5K, input voltage 9V…
Part Number: TL431-Q1 Tool/software:
Dear TI Team,
I looking for calculation of worst case voltage deviation of TL431B-q1 in the temperature range 10°C to 50°C. Full temperature range shows 34mV max deviation.
Thanks!
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431 Hello Experts,
Is there an particular reasons for using 27.4 kOhms value ? any value for this resistor, satisfying Vo-Vin relation can be used, right ?
Part Number: TL431-Q1
1.Please let us know the difference between T L431BQDBZRQ1 and TL431BQDBZR.
Does these part use same die ?
Only Automotive Qualification ?
2.We found the difference of ESD rating between these 2item.
Please let us the…