Part Number: TL431LI-Q1 Other Parts Discussed in Thread: TL431 Hello team,
Customer want to use TL431LIAEDBZRQ1, some application questions are as below:
1) The output is 2.5V. Does TL431 have any requirements for the voltage drop between input and output…
Part Number: TL431LI-Q1 Other Parts Discussed in Thread: TL431 , TL431LI Hello TI Engineers,
I am using TL431LIBQ to design the feedback compensation network for single switch forward converter. I have two questions in this regard,
1. In the datasheet Fig…
Part Number: TL431LI Hi team,
In the figure 7-3 and 7-4, it says VKA=VREF at the lef top of the graph.
But VKA is variable in the charactoristic.
What does VKA=VREF means in this grapf?
Does it mean VKA_max=VREF?
Also, I want a explaination for the meaning…
Part Number: ATL431LI Other Parts Discussed in Thread: TLV3502 , , TLV431A , TL431 , TLV431 , ATL431 Hello,
I currently use the TLV431A to generate a reference voltage of 3.225 for the TLV3502 component, from a voltage of 3.3V using the circuit described…
Part Number: TL431LI-Q1 Hello team e2e,
One of my customers is working on this Model in Simetrix for the Recent revision of part TL431LI-Q1
They would like to have SIMPLIS model to do the stability Simulation
Do we have this ? If not, do you know if Unencrypted…
Part Number: TL431LI Hi Reference Experts,
for TL431LI in the DS the continuous cathode current is specified with a max value of 18mA.
Do we have some data for short term load ?
My customer is looking into short loads up to 21mA for ~1ms.
Normal continuous…
Part Number: TL431LI Other Parts Discussed in Thread: TL431 Hi,
Why Iref value on TL431LIB is big different from Iref pf TL431AI? Please advise us.
TL431LI
TL431AI
Thanks and best regards, M.HATTORI.
Part Number: TL431LI-Q1 Other Parts Discussed in Thread: TL431LI , ATL431LI , ATL431 Hi team,
May I know what is difference between TL431LIBQDBZRQ1 and ATL431LIBQDBZRQ1?
In ATL431LIBQDBZRQ1, it needs less Ika current 80uA compared with TL431LIBQDBZRQ1 6mA. …
Part Number: TL431LI-Q1 Hi team,
Could this device operate with 125C<TJ<150C? Its datasheet "7.3 Recommended Operating Conditions" and "7.5 Electrical Characteristics" just mention TA instead of TJ. Should we use TL43xLIxE-Q1 …
Part Number: TL431LI Hi Team,
My customer is considering to use TL431LI to generate 3.3V power supply for RTC which requires less than 10uA.
I was asked to review their following schematic though, could you help that?
They mind CL is enough to get stable…