Part Number: TL432LI Other Parts Discussed in Thread: TL431LI Tool/software: Hi,
Please tell me the accuracy of Vref (min/typ/max) or Vref (min/typ/max) when used under the following conditions.
<conditions>
IKA=5~6mA, VKA=3.161V, Vref=2.5V
In…
Part Number: TL432LI-Q1
Tool/software:
Hello experts,
I am Erick, sales in Taiwan, I would like to kindly request for your help with analyze or give me any feedback if there could be any risk to put TL432LIBQDBZRQ1 in immersion cooling.
The…
Part Number: TL432LI Other Parts Discussed in Thread: TL431LI Hi Expert,
According to TL432LI item 10.2.1.1 design examples:
The TL432LI can operate under 2V on VKA .
Pls help to why it works, and any requirements need if need the VKA under 2V…
Part Number: TL432LI-Q1 Dear Team,
as per firgure 1 in datasheet there is a non-linearity. High at ambient temp and lower Vref when temp goes up or down.
Can one assume that this behavior/pattern is the same for all parts we ship to the customer or…
Part Number: TL432LI Other Parts Discussed in Thread: ATL431LI , TL431LI My client wants to use TL432LI for LA431, IKA parameters are as follows, will there be any side effects?
TL432LI IKA: 1mA~15mA
LA431 IKA: 0.3mA~100mA
Part Number: TL432LI-Q1 Other Parts Discussed in Thread: TL431LI Hello,
Can you confirm the cathode current requirement (IKA) at VKA > VREF working condition? Is this 1mA? Also provides the calculation for finding Vref for this application
Regards…
Other Parts Discussed in Thread: TMP61-Q1 , TL432LI , LM334 , TMP61 , TL1431 , INA500 Hello E2E Community,
We are evaluating low-cost alternatives to the typical voltage divider configuration when using the TMP61-Q1 in our application. Our setup involves…
Part Number: ATL432LI Other Parts Discussed in Thread: TL432 , TL432LI , , ATL431LI Hi, Because the TL432 and TL432LI are out of stock, and ATL432LI we has stock, so I want to use ATL432LI to replace the LA431OCRPA, and the datasheet as the following…