Hi Marvin,
as we have not received an additional information, I assume this issue is solved and I am closing the thread. If there is still something open, just reply to open it again or open a new thread.
Best regards, Stefan
Part Number: TL497A Good Day. Apologies in advance for asking about such a venerable part. It is still in current production in lots of packages, though, so there is demand and field use of the part.
Some documentation refers to protection circuits which…
Part Number: TL497A Other Parts Discussed in Thread: TPS55340 Hi,
we are looking for 5V input +/-10V output 500mA solution. Any suggestion? thanks!
PY Tsai
Other Parts Discussed in Thread: TL497A I am trying to generate -0.5V (0.1A) using TL497A. Is this possible with this regulator? because the calculations give me a negative R1 resistance value. Please suggest alternatives if not possible
Other Parts Discussed in Thread: TL497A , MC34063A Hi,
I have a TL497A set up to convert +5V to -19.5V. The problem I am running into is that the output voltage drops to -14V or so when the load is greater than a few mA. I need to be able to supply ~20mA…
Other Parts Discussed in Thread: TL497A Got some 20 really old bugs: TL497CN and most of them with date code 7624 and stamped 72497 on the bottom side.
My question:
What is the difference between this TL497 and the present-day TL497A, please? Enlarging…
Other Parts Discussed in Thread: TL497A Hello all,
My design requires a minimum of 1.5 A current, I want to be able to boost my 9V lithium ion battery to about 18 Volts output voltage and get a minimum of 1.5 A output current from the TL497A chip. I have…
Hi!,.. i don't know if this is the correct post but i will tell my doubt.
I'm trying to design a 20V 500mA output voltage source with a 5V input, using the TL497A. I'd design with the equations in page 5 using the circuit with external transistor…
Other Parts Discussed in Thread: TL497A Hi: I'm using the TL497A and would like to use the same type of part (COT), but at a higher operating frequency, as to reduce the component size. Low ripple is a must. I need a part to convert +15 vdc to -15vdc …