Part Number: TL598 Hi sir,
My name is Santhosh.
I want to use TL598 pwm controller for some application.
I studied TL598 applications thoroughly and got confusion about positive feedback section.
Why positive feedback section is implemented for error…
Part Number: TL598 Hi sir,
My name is Santhosh.
I want to use TL598 pwm controller for some application.
I studied TL598 applications thoroughly and got confusion about positive feedback section.
Why positive feedback section is implemented for error…
Part Number: TL598 1. Downloaded TI PSpice program expecting to see TL598 in the PSpice library. Apparently not. Also can't find any PSpice reference in TL598 data area. Help.
2. Have been using TL598 for 20ish years to drive a constant current source…
Part Number: TL598
Hello
Is there a problem with connecting a buffer operational amplifier to the output voltage feedback line when connecting the error amplifier of the TL598? This is to feed back the output of the negative power supply.
Thanking you…
Part Number: TL598 Hello Is it possible to input the comparison reference voltage from the outside when connecting the error amplifier of TL598? This is because the voltage is variable by an external signal. Thanking you in advance.
Hi,
Since the TL594 is only functionally equivalent to TL598. The graph you are asking for is not available. I recommend to test the TL594 and characterize it's performance against your requirements.
Steve
Part Number: TL598 Dear, we have been using the TL598QD for many years and we recognized now that is offered only commercial version with operation temperature 0°C to +70°C .We are able measure our electronics assembled by TL598CD in temperature…
Part Number: TL598 Dear, we have been using the TL598QD for many years and we recognized now that is offered only commercial version with operation temperature 0°C to +70°C .We are able measure are electronics assembled by TL598CD in temperature…
Other Parts Discussed in Thread: TL494 , TL598 Dear Sir,
Can I use TL598CN in place of TL494 for pushpull configuration ?
I need to use inbuilt 200mA Mosfets as push-pull switches.
Re,
Parth Patel