Part Number: TL751L Hi,
I'm using the TL751L05CD on one of my designs as a simple signal invertor and level shifter. It should be as simple as pulling a 12V signal low and seeing a 5V output however I get an output of around 9V.
I've already tried…
Part Number: TL751L Other Parts Discussed in Thread: TL750L , LM2936 , LM2931-N This part is to be used in our design as an alternate part for the TL750. Our design does not tie the enable disable pin to enable. The datasheet does not say if the enable…
Part Number: TL751L Other Parts Discussed in Thread: LP2960 , LP2954 , LP2954A , Does there exist a cross for the TL751L05CDR which has more current output?
This one is 150mA, I need over 200mA
Part Number: LM2936 Other Parts Discussed in Thread: TL750L , TL751L , LM9036 , UA78L , Dear Sir,
I am using LM2936MP-3.3 in my PCB.
My circuit output voltage is shifting to 100mV up. Initially, my output voltage is 3.25 VDC after turning on the 12V…
Hello Rhino,
The ADS1243 digital supply minimum speed for proper Power On Reset is 1V/10ms. If the voltage supplies ramp up slower than this rate there are two potential issues:
- The One Time Programmable register values containing some of the…