Part Number: TL7660 Hi,
We have a product in development which uses the TL7660 to increase the voltage supplied from a high-impedance source. The voltage source is a regulator in series with a 150 ohm resistor. The datasheet (page 8) suggests that there…
Part Number: TL7660 Hello, I am trying to generate -5V using TL7660. I am using 2 capacitors (c1 and c2) 10uF tantalum type same as the datasheet suggested (C1 positive is with pin 2 and C2 positive is grounded). But when I am providing +5V or +3.3V in…
Part Number: TL7660 Other Parts Discussed in Thread: TINA-TI , Hallo expert,
I want to us TL7660 charge pump converter to converter 3.3V to 14.5V. Can you help me to check following circuit ? Can you provide a simulation model of TL7660 in TINA-TI or Pspice…
Part Number: TL7660 On a follow-up question, I am trying to get a negative output voltage in the range of -0.25 VDC to -0.75VDC using a positive PWM DC Input using a TL7660. This does not seem to work. If I connect a battery, the output converts to negative…
Part Number: TL7660 Other Parts Discussed in Thread: TPS65135 , LM2664 , TPS60401-Q1 Does the application team have a Pspice deck available that supports the TL7660 "Figure 10 Negative - Positive" combination that I could run in PSpice for TI?…
Part Number: LM2776 Other Parts Discussed in Thread: TL7660 I am planning to use LM2776 for VInput of 5.8V max. The operating ranges states is only 5.5V. but abs max is 6V. Please can you comment if it is okay.
Please can you also confirm that if TL7660…
Part Number: TL7660 Hi team,
My customer is trying to use TL7660 to generating -3.6V from input 1.8V.
They try the solution using 2 units of TL7660 as datasheet Page 11, figure 6.
do you think the pin8 is connecting to Ground, or it needs to connect to…