Part Number: TL7700 Other Parts Discussed in Thread: TPS3422 , TPS3424 , TPS3435 Tool/software:
Can I generate a fast reset pulse like that shown below using the TL7700?
Thank you
Part Number: TL7700-SEP Hi,
I want to use the TL7700-SEP as a Power-on-reset IC (POR). The system description is as shown in the attached file.
The MCU on the main unit is connected via 2meter cable to a remote unit with TL7700-SEP device.
The two…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3842 , TPS3808E Tool/software: We plan to monitor the power supply with the TL7700. Could you explain the concept of tpo? In the data sheet, the tpo section states that when Ct = 0.01uF, it is 0…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3842 , TPS3808E Tool/software: 電力監視でパルス幅を決定するコンデンサについて教えてください。
Ctの両端の電圧はどれくらいですか?
Vccか、SENSE電圧か、それとも他の何かですか?
Part Number: TL7700 I would like to know the recommended input voltage range for the SENSE terminal. The absolute maximum rating in section 6.1 is –0.3 V to 41 V, but what is the recommended range? In section 6.5 Electrical Characteristics, the specification…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3842 Hello, My customer would like to use TL7700 at Vcc=12V. At the CT pin, they would like to use as small size capacitor as possible. At the minimum, what voltage rating capacitor should be used…
Part Number: TL7700 Hello team,
Will the RESET pulse width be which is set by CT cap, even if Vcc is lost?
My customer will tie Vcc and SENSE, so if customer would like to know if the RESET pulse is going to be out even when Vcc is lost.
Best Regards…
Part Number: TL7700-SEP Tool/software: Hello - I am using the TL7700-SEP as a supply supervisor, as shown in Figure 9-1 of the datasheet. I'd like to add a filter capacitor from SENSE to ground (i.e. in parallel with the 30k R2 resistor). I'd think this…
Part Number: TL7700 Hi,
Could you provide a simulation model of TL7700? I would like one of the following two models. ・PSpice model (extension .lib) ・IBIS model (extension .ibs)
Thanks,
Conor
Part Number: TL7700 Tool/software:
Hello team
Customer woul like to get TL7705CPSR-B datasheet, but we dont find it in TI.com.
Could you share us TL7705CPSR-B datasheets?
Thanks