Part Number: TL7700 Other Parts Discussed in Thread: TL7705CPS-B , Hi,
I am considering the TL7700CPS as a replacement for the TL7705CPS-B.
Q1. Could you tell me the specific differences?
Q2. Please let us know if you have any concerns about the replacement…
Part Number: TL7700-SEP
The TL7700-SEP datasheet (SLVSF13A Rev August 2021) shows that the SENSE input current (I s ) ranges from 1uA to 3.5uA over temperature, with a typical value of 2.5uA at 25C. That means even if I have perfect resistors in my voltage…
Part Number: TL7700-SEP In which direction is the hysteresis voltage applied?
Based on Figure 8-2 (attached) of the from the TL7700-SEP datasheet (SLVSF13A Rev August 2021), it appears that Vhys is applied on the upward edge of the SENSE input. I.e.,…
Part Number: TL7700 Hello team,
I received a question from the customer. When resetting by an external switch, is it correct to connect the reset signal to the CT pin?
Regards,
Masa
Part Number: TL7700 Hi,
Can you clarify what is meant by "If the sense voltage (Vs') does not have hysteresis in it, and the voltage on the sensing line contains ripples, the resetting of TL7700 is unstable" in the datasheet?
Does this mean…
Part Number: TL7700 Hi team,
Customer wants to understand the tpd when the RESET wolud fall.
The tpd is 10usec(max) according to the datasheet.
- Is the 10usec ture for the falling?
- Is the tpd varied CT? They use 4.5uF as CT. In this case, could you…
Part Number: TL7700 Other Parts Discussed in Thread: TLV840 Hi Experts,
My customer is evaluating TL7700. The reset pulse duration is not expected one. Below is the schematics.
10uF is connected at CT pin so the expected reset duration is around 1sec…
Part Number: TL7700-SEP Hello Team,
The datasheet of TL7700-SEP states that this is • Radiation hardened: – Single event latch-up (SEL) immune to 43 MeVcm2 /mg at 125°C
Since there is no data relevant to other SEE (e.g. SET), can we consider…