Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TL7700 Other Parts Discussed in Thread: TPS37
Hi team,
My customer will use TL7700 for their application and they're asking about tolerance(min-max) estimation of tpo.
According to datasheet, tpo can be calculated as tpo=Ct*10^5 second…
Part Number: TL7700-SEP Hi,
The minimum component height is not listed on the drawing for this part (TSSOP (PW)). Is this information available? We are looking into using thermal gap pads and need min height for this.
Thank you!
Lincoln
Part Number: TL7700 Hi,
I have a question about the IoL on the RESET pin.
Customer request: Under the following conditions
Operating temperature: -10 ° C to + 60 ° C VCC: 12V ± 1V
They need an IOL value that the VOL of the RESET pin is less…
Part Number: TL7700
Hi,
Our customer has two questions.
Q1 When the CT is discharged due to a drop in the SENSE input voltage, if the SENSE input voltage is restored before the CT discharge is completed, the pulse width of the RESET output will be shorter…
Hello,
This device is not radiation tested. The best alternative with radiation data is : TL7700-SEP data sheet, product information and support | TI.com
Part Number: TL7700 Dear TI Team
Our customers are considering the TL7700
They are trying to use a 0.1μF, withstand voltage 16V capacitor for the CT pin. From the following post, the voltage of the CT pin is usually about 1.5V, so I think that there…
Part Number: TL7700 Hello,
my customer has observed incorrect operation of hysteresis.
Their setting and expected operation are below
R1: 240K ohm, Vs=3.5V, reset asserts when voltage goes down less than 3.5V
R2: 40K ohm, Vhys=0.6V, reset release when…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3710 Dear Support,
I would like to use the TL7700 to monitor a 12V rail. The RESET should trigger if the input voltage drops anything below 9V. I am struggling to determine the resistor values required…