Part Number: TL7702A Tool/software: Hello,
The example circuit might have a potential mistake that could damage the device.
The RESET output of the bottom TL77 is connected through a 10 kohm resistor that limits the current through the diode…
Part Number: TL7702A Other Parts Discussed in Thread: TPS37 Hello guys. Could you tell me the evolution for the CI TL7702AD? I would like to upgrade my project to a more current CI.
TRANSLATE with x
English
Arabic
Hebrew
Polish…
Part Number: TL7702A How can I see the sub components that make up this chip TL7702ACD. I'm performing a equivalency evaluation of another device and would like to know whether there are diodes, transistors, resistors, etc that are used on the TL7702ACD…
Part Number: TL7702A Hi All,
I have a question about TL7702A.
Is it possible to use the REF pin as an external power supply? When used as an external power source, the load current is 100uA. Is it possible to operate normally?
Best Regards, Ish…
Mario,
The TL7702A was created in 1983 and TL7702B was created in 1989 so that could explain the improvement of Iq spec from version A to B. I can verify on the bench and let you know what I find.
-Michael
Other Parts Discussed in Thread: TL7705A On attached TL7705A datasheet P2, writing about Internal resister of SENSE-Pin.
TL7705ACP.pdf
I substituted and calculated Vref:2.48V~2.58V (and TL7705's R1,R2).
As a result, VIT-:4.41V~4.59V.
It's difference…