Part Number: TLA2022 Other Parts Discussed in Thread: ADS7142 Dear *,
Can we connect the I2C of TLA202x to 1.8V with pull-up?
Our system i2C is 1.8V, and we would like to avoid the level translator.
if no what low-cost ADC solution do you suggest that…
Part Number: TLA2022 Other Parts Discussed in Thread: ADS1015 , Hi there,
My customer is asking for a cheaper version of ADS1015 and I found TLA2022 should be the one.
However, I'm wondering what are the differences between the two?
At first glance…
Part Number: TLA2022 Other Parts Discussed in Thread: ADS1120 , ADS1231 , ADS1131 I am trying to design a weight scale to measure parcels with a 0.02 lbs accuracy, to measure upto 50 lbs.
I am using weight/load sensors from Aliexpress which are half bridge…
Part Number: LMT70 Other Parts Discussed in Thread: TLA2022 When using a 'scope to probe the LMT70's output, the voltage drops somewhat. We can determine this because we have an ADC (TLA2022) and firmware reporting the output.
The probe is 10…
Jason,
For a measurement of 0V to 3V, you would need to use the PGA, and therefore use the TLA2022. The TLA2021 only can be set to a full scale range of ±2.048V. For something larger in the TLA2022, you could use the ±4.096V range. Note that the ADC…
Part Number: TLA2021 Other Parts Discussed in Thread: TLA2022 Hi all,
I have a question on TLA2021.
In the data sheet pin function (1), Unused pins may be connected to GND or open. "Float unused analog inputs, or tie unused analog inputs to GND."…
Part Number: TLA2024 Other Parts Discussed in Thread: TLA2022 Dear sir,
I plan to use the TLA2022/4 to monitor the voltage and current of USB A interface. the voltage and current input range is different. Can I set different PGA gain for different channel…
Which ADC should I use for my analog temperature sensor? Can I use the internal ADC of an MSP430 or SimpleLink MCU? (i.e. MSP432, CC2652, CC3220/CC3235 or CC1352)