Hiroki Nishimoto said: > As I mentioned before, I'd also like to see the voltage level of VDD during the error if you could capture that as well.
The attachment is an enlarged image taken at the time of the issue occurrence. You should be able to…
Part Number: TLA2024 Section 8.5.2.1 in the TLA2024 data sheet only shows I2C reads using stop followed by start (after the register pointer and before the read command). However in the I2C timing requirements, section 7.6, there are values for repeated…
Part Number: TLA2024 Example Board Layout wrong measurements wrong:
In the TLA2024 Datasheet page 34 the total measurement of the suggested Footprint is 1.85mm. But the sum of 0.58mm + 0.58mm (for both pads) and the distance between the two pads 0.7mm…
Part Number: TLA2024 Hi TI service team,
This is Paul from ZT hardware team.
To be more clearly, we utilize these two AIN pins (AIN0 and AIN1) for voltage sense ( actual voltage from mutimeter on board: 1.6v~2.82v ) and convert this value (must a positive…
Part Number: TLA2024
Hello,
We need to confirm our observations:
1. For TLA2024 If we configure input multiplexer AINP = AIN0 and AINN = AIN1 we are not able to read correct differential output. Is it recommended to use AIN0 & AIN1 channel for differential…
Part Number: TLA2024 Other Parts Discussed in Thread: , ADS1115 Hi Experts,
Our customer would like to ask if it would be possible to communicate with TLA2024 via I2C-to-USB adapters like https://www.adafruit.com/product/4471 for debug purposes using your…
Part Number: TLA2024 Other Parts Discussed in Thread: ADS1015 Hello,
We are reading adc value for input ac voltage of 1.5v on channel AIN0 and 2.2v on channel AIN1 in differential mode. We are reading peak to peak values and verified it on oscilloscope…
Part Number: TLA2024 Dear Sirs.
Could you let me know why ESD test is not performed in the Qualification report of PCN#20221219004.1?
ESD test can be found in PCN#20221219007.1 and PCN20221216004.1 issued at the same time.
Best regards.
Tsuyoshi Kanakogi…
Part Number: TLA2024 Hi,
My customer use TLA2024 for new project’s openbmc FW development.
They only find the iio driver for TLA2024, does the device have hwmon driver support for openbmc?