Part Number: TLA2518 Other Parts Discussed in Thread: SN74LVC1G125
I'd like to connect 10 TLA2518 devices to a a single SPI bus. The datasheet does not specify pin capacitance or max load capacitance for the SDO pin.
Should I buffer the SDO pin with…
Part Number: TLA2518 Where are the code examples this part?
I read another post a similar question, and TI's response was there are none.
I have to say that's ridiculous!!! Obviously you had to write code to test it, so share it.
The data sheet…
Part Number: TLA2518 The task is to convert an input six times in a row as quickly as possible. This raises the question of whether the "Auto-Sequence Mode" also works with a single input?
Hello Cynthia,
My takeaway from your reply is that tack_min (400ns) is not a strict limitation, but is malleable depending on the input drive circuit.
Please help me understand exactly what you are referring to with the 'input drive circuit'. Are you…
Part Number: TLA2518 Hi team,
In the TLA2518 datasheet there is no mention that I can find of the calibration time. For calibration, all I see is what is given in 7.3.4:
The variation in ADC offset error resulting from changes in temperature or AVDD can…
Part Number: TLA2518 Other Parts Discussed in Thread: ADS7038 , ADS7028 When configuring Channel 0 as a GPIO, the pin does not function as expected.
When configured as a GPIO push pull, the pin is always high; and when GPIO0 is configured as an open drain…
Part Number: TLA2518 Section 7.4.3 of the datasheet demonstrates an on-the-fly mode transaction between a master SPI device and the TLA2518.
5 bits are required at the start of a cycle to specify the next channel to sample.
The first bit is shown to always…
Part Number: ADS7038 Other Parts Discussed in Thread: TLA2518 , , ADS7028 Hi team, I'd like to consider TLA2518. However TLA2518 does not have EVM, so I should use ADS7038Q1EVM. I think ADS7038 mainly added the CRC from TLA2518. Are there any other different…
Part Number: TLA2518 I am having an issue with Channel 0 as a digital Push-Pull output.
When I configure Channel 0 to a Digital Push-Pull output it is always HIGH. I cannot set the output to a LOW level. I can successfully use the other channels (1-7)…
Part Number: TLA2518 Hi Team, we want to confirm if this is possible.
Is it possible to keep the CS line low during acquisition with TLA2518? Using it in DMA-continuous mode and microcontroller doesn't provide a convenient way to rise CS after each conversion…