Part Number: TLC2272 Hi! I have M-Audio sound card and it was malfunctioned. I need a this integrated circuit. I'm jut asking for be sure. which one should I choose from the list. I2m a just musician and i must found this piece Thanks for understanding…
Part Number: TLC2272 Other Parts Discussed in Thread: TLV2772 Hi team,
My customer now use the TLC2272 to do the current-sensing from the compressor of the Air conditioner and the frequency of the current detected in EM_SENSE is several tens of KHz.
…
Part Number: TLC2272 Other Parts Discussed in Thread: OPA196 Dear Team,
we understood from some E2E posts that the TLC2272CPW has some advanced ESD at the inputs. Our customer has some questions about the internal clamp diodes:
Does the TLC2272CPW have…
Part Number: TLC2272 Hi,
I had made a simple buffer circuit from the TLC2272 (V+= 3.3V, V-=0 ) . The input to the IN+1 pin is +1.25V DC from a 100k potentiometer. The output shows the DC voltage (1.25V) + a 100mV pk-pk noise with a frequency of 1Mhz. …
Hi Marek,
Thank you for answering.
How come the datasheet doesn't say directly that the Y axis correspond to the phase margin?
For someone who is not really used to op amp, it can be very confusing and not straightforward to guess that in some datasheet…
Hello Suraj,
Do you have all the information you need to move forward with your TLC2272 application? If so, please close this e2e inquiry.
Regards, Thomas
Precision Amplifiers Applications Engineering
Part Number: TLC2272 I would like to know if there is any data that can be shared on the typical channel-to-channel crosstalk performance up to about 20kHz?
Thanks,
Rob D'Angelo
Part Number: TLC2272 Hi team
Datasheet says that the absolute maximum is VDD+<8V and VDD-<-8V.
Is it damaged to device if VDD=9V and VDD=0V is applied?
Regards,
Saito
Carolina
Attached Schematics as well as repeatability results of 25/07/2023 report.
Simulation of TINA also shows linearity but there is a saturation at 4V not swing up to +5V. Have sent this to you by email for TLC2272 IAR Report OPA499ID_25072023.pd…
Part Number: TLC2272M Other Parts Discussed in Thread: TLC2272 , TLC2272A
Hi Colleagues,
I have a few queries regarding the TLC2272M, to which I need some clarification. The datasheet in question is this one .
Two parameters are given for the input offset…