Part Number: TLC339 Hello, I am looking at the circuit on page 50 of this presentation ( Microsoft PowerPoint - Sec2_RemoteSysMonitor_Print.ppt (ti.com) ). I am unable to understand the reason for use of this battery and the 2k resistor here. Would really…
Part Number: TLC339 The pulse was extended without reason from the input comparator to the output (8msec pulse from the input has prolonged to 44 msec at the output).
Is there any answer/reason for that?
Recently, our system was failed because of 5 faulty…
Part Number: TLC339 Hi team,
Good day.
Our customer would like to know the HBM, CDM and MM ESD rating for the following devices:
LM6511IMX NOPB
TLC339IDR
TLC339IPWR
TLC3704IPWR
TLC393IDR
Thank you in advance for your help.
Regards, Carl…
Part Number: TLC339 I am using TLC339 comparator in one of our circuit with the VCC=3.3V and GND. I have attached the schematic. The input is a square wave with frequency of 100Hz and amplitude is +/- 15V.
When the input is -15V the diode will be forward…
Part Number: LM139A Other Parts Discussed in Thread: LMP7300 , LM2903B , LM2903 , TLC339 Hi Experts, Good day. Please help provide the temperature drift characteristics of the LM139A voltage comparator.
Keep safe. Regards, Josel
Power the comparators from −5 V and 5 V (or something higher). Connect the input signals to the inverting comparator inputs, and a reference voltage of about 2.5 V to the noninverting inputs. Connect the pull-up resistors at the outputs to GND. …
Other Parts Discussed in Thread: TLC374 , TLC339 , TLV3401 , TLV3701 Dear support,
I am looking for the value of the input parasitic capacitance for both the TLC339 and TLC374 - this is not shown in the documentation
Thank you - Yves Camille - Arrow El…
Other Parts Discussed in Thread: TLC339 This question is being posted for an FAE:
For TLC339, I have a question:
If the VDD is powered by 5V and we have got a pullup resistor on the comparator output pin that is pulled up to 3.3V. Is that OK? Does the…
Other Parts Discussed in Thread: LM339-N , LM339 , LMC7215 , TLV3691 , LPV7215 , TLV3701 , TLV3401 , LP339 , TLC339 , TLC3704 , REF3325 , REF1112 The Output sink current of LM339-N is specified as 6mA min.
Since this part has an open collector output, does it mean…
Other Parts Discussed in Thread: TLC393 , TLV1702 , TLC352 , TLC339 , TLC372 , TLC3702 Hi,
We are considering output voltage is unexpected when low VDD.
The output voltage should be low on this condition.
What is the VDD voltage to change output voltage high…