Part Number: TLC59108 Hello.
I have been studying the 59108, 59108F, and the 59208 parts. I saw the following information in the data sheet for the 59108 and 59108F: Constant Output Current Adjusted Through an External Resistor (10mA to 120mA)
and then…
Part Number: TLC59108 Tool/software: Linux Hi support team
Can I send i2c command into TLC59108 that behavior is a Breathing light ?
Thanks and Best Regards,
Part Number: TLC59108 Hi, team.
When TLC59108 is used in parallel as shown in the data sheet Fig24, flicker occurs.
What would be your first advice when troubleshooting?
Best Regards,
Part Number: TLC59108 Other Parts Discussed in Thread: TLC59116 , I had trouble getting this part to work too. Moving from TLC59116 code which worked fine. As from the datasheet both parts are controlled the same way apart from some obvious changes in registers…
Part Number: TLC59108 Hi
Problems are occurring at customers.
The customer concurrently controls OUT 0 to OUT 7 using the GRPPWM register of TLC 59108. The duty of GRPPWM is controlled from the host to the TLC59108 at intervals of 5ms. However, duty is…
Part Number: TLC59108 Hi
My customer has question.
The customer wants to use TLC 59108 and simultaneously control LEDs 0 to 7 with GRPPWM.
How can I control with GRPPWM?
Best Regard
T Kishi
Part Number: TLC59108 Hi,
I dont think i seem to understand TLC59108IRGYR.
The constant current sink is used set the current.
Is analog dimming used according to the GRPPWM register value on channels?
Please explain how TLC59108,REXT,PWM register all links…
Part Number: TLC59108 Hi,
I have been asked to find out if this component we purchased has embedded firmware. Additionally, I need to know who manufactured the firmware and where it was manufactured, if it is embedded. The part number I have is TLC591…