Hi Stefan,
"This E3E topic describes that the difference between TLC59108 and TLC59108F are just the output structure. (Current-Source / Open-Drain)"
Please note that they are the main difference between TLC59108 and TLC59108F, rather than TLC59108F…
Part Number: TLC59108F I have got a problem with the TLC59108F LED Driver: There is a LED connected to LED7 output port which should change blinking frequency every five seconds from slow to fast and back.
It starts blinking slow and then stops blinking…
I used the allcall to address it, the Arduino "wire" library has some limit on addresses, and it crashes if the address is above 127.
As it turns out, that addressing issue caused me to look deeper into it, and I found my [user-error] ... ugh... I was…
Other Parts Discussed in Thread: TLC59108F , TLC59108 Hi all Would you mind if we ask TLC59108F and TLC5910? What is the difference between TLC59108F and TLC59108? It seems that there is only LED Open Detection, but if you have some information, could…
Other Parts Discussed in Thread: TLC59108F Hi Team,
Our customer are evaluating TLC59108F.
However, the high frequency noise(peak frequency is 180MHz)* occurs on Vcc line.
Therefore, they would like to ask about the following questions.
*…
Other Parts Discussed in Thread: TLC59108F , TLC59108 Hi,
I am trying to make my new design work using a TLC59108F.
Using I2C bus, I can write the reset bus command and I can also write to any internal register and they all read back OK.
Nevertheless…
Part Number: TLC59116F Other Parts Discussed in Thread: TLC59108F Hi support team,
Confirmation of tSU;STA specification of I2C Interface of TLC59116F. The MIN value of STANDARD-MODE of SCLS714C is 1.7μs.
In the following document of NXP, it is…
Hi Anthony,
Please refer the below comment.
: Could you please confirm that "constant current" really means that the current on given output (OUTn pins) will be kept constant for a given step? The datasheet is not very clear. "constant current" seems…