Part Number: TLC59116 Hello,
I want to drive a led like H455CBC which have two leds in antiparallel configuration. Is it possible to drive these leds by using two channel of the TLC59116 and connecting pull up resistors to both channels ?
Best…
Part Number: TLC59116 Other Parts Discussed in Thread: LP5812 , TCA9539 Hello,
I want to drive a led like H455CBC which have two leds in antiparallel configuration. Is it possible to drive these leds by using two channel of the TLC59116 and connecting…
Part Number: TLC59116-Q1 Hi team,
The customer is considering the TLC59116-Q1 quiescent current in their battery products
It seems that the TLC59116-Q1 will have 25mA even when the LED are all off
Is that possible to pull-low the /RESET to reduce…
Part Number: TLC59116 We would like to use TLC59116 in our application. However, our I2C bus has another device on it which uses address 0x68. This conflicts with the TLC59116 All-Call address.
Per the datasheet, the TLC59116 All-Call function is enabled…
Part Number: TLC59116 Tool/software: Hi,
What is the OFF state current of the OUT pins?
Even though all LED driver x , LDRx=00 of LEDOUT0/1/2/3 registers are OFF , the LEDs are still on with very dim light.
The white LED is Cree XD16 that supports…
Part Number: TLC59116 Tool/software: We are considering using the TLC59116 to control multiple RGB LED elements with a constant current.
The Io specifications are listed in 7.3 on page 6 of the datasheet.
It states that out0 to out15 are Min. 5mA…
Part Number: TLC59116 Tool/software: Dear Support,
Our company using since several years part TLC59116IPWR. Shortly we have problems with this part that the LED connected to IC is burned (damaged). Nothing is changed in the design.
The LED we are…
Part Number: TLC59116 Hi team, Could you pls help with the following questions about the tlc59116:
1. Is the output of this IC in the default high-impedance state when it is powered on?
2. What is the voltage drop of the IC's out pin when the light…