Part Number: TLC59116 Tool/software: Dear TI-Team,
I had the following support discussion with you some time ago.
e2e.ti.com/.../tlc59116-driving-mosfets-with-the-outputs-of-led-driver
Unfortunately, I was not aware that the request would be publicly…
Part Number: TLC59116EVM-390 Other Parts Discussed in Thread: TLC59116 , USB-TO-GPIO2 , USB2ANY Hello TI Support Team,
I’m bringing up a TLC59116 EVM and running into an interface issue:
Setup
EVM powered from bench supply via J4/J5 at 5.0 V…
Part Number: TLC59116 Tool/software: Hi team,
I want to confirm about RESET pin connection.
seeing following figure, there is no need of external pullup, but seeing datasheet 9.3.4, it says RESET pin need external pullup.
The figure is rough example…
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: TLC59116 Tool/software: Heya there,
I have recently had a PCB made to test out the TLC59116 with some LED's, including pushing it up to max power (120mA current per channel) to try and push 2000…
Part Number: TLC59116 Tool/software: Hello, My customer plans to use TLC59116 now. They would like to light up the LEDs gradually and also turn off the LEDs gradually. To do this, do they have to control the duty of the PWM step by step? Any other recommended…
Part Number: TLC59116 Tool/software: Hi experts,
Do you have any resource for software development?
ex: library, sample code, etc.
Thanks and regards,
Tsuyoshi
Part Number: TLC59116 Hello,
What is the minimum value for Vo for the TCL59116? In the datasheet, the max voltage is 17V, but there is no min in the spec.
Thank you,
Kyle
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: LM3509 , TLC59116 , TPS92512 , LM3410
Tool/software:
Hello TI Team,
We are looking for an infrared laser diode driver or a constant current LED driver.
Input Voltage Available:5V We would…
Part Number: TLC59116-Q1 Tool/software: Dear team,
Can I know how to set different output current for each channel?
In case we want to set different output current for each channel (e.g. using different color) - Is the below process correct?
1.…