Part Number: TLC5916 Other Parts Discussed in Thread: TLC5940 , Facebook has an array of LEDs and are looking for a driver, rough spec below. The most important feature is low noise in the current output.
LED Driver spec
Constant current with one…
Part Number: TLC5916 Other Parts Discussed in Thread: SN74AHCT594 ,
Hello,
I want to cascade as many as 8 SN74AHCT594 shift registers (for general purpose digital outputs) and 3 TLC5916 shift registers on the same serial interface. Serial Clock rate should…
Part Number: TLC5916 Other Parts Discussed in Thread: TLC5927 , TLC5926 , , TLC5917 Dear TI,
Is it possible to get PSPICE model/testbench from one of this drivers: TLC5916,TLC5917,TLC5926 or TLC5927?
I want to simulate the driver together with TLC555D timer…
Part Number: TLC5916 Other Parts Discussed in Thread: TLC5954 TLC5916_Special mode_error__20180329.pptx Dear all
Concerning TLC5916, I have some problem.
Normal mode is good work but it is not enter to special mode.
(CLK,_OE,LE clock is same as datasheet…
Part Number: TLC5916 On the testing TLC5916, output current is set 15mA by configuration, but test result was 10mA.
Please let me know about why output current was differ.
Test condition is below;
・VDD:5V, 100Ω load
・Control signal(by FPGA) is…
Part Number: TLC5916 Please let me confirm about correct data sequence, MSB First or LSB First.
When set LSB First, test data was fine.
But I look like MSB First by datasheet page-20(attached), is this misread?
Which is correct MSB or LSB?
Best regards…
Part Number: TLC5916 Other Parts Discussed in Thread: TLC59282 Hi,
I have problem in setting the current configuration code correctly. It seems that even if I change the current configuration value to diffrent values it always seems the same.
I followed…
Part Number: TLC5916 Please let me know about Minimum Vout spec for TLC5916(and the other LED Driver).
I think that when VDD: 5V and Voltage drop by LED: 4V, TLC5916 supply is 1V, is it correct?
Is there the other points of notice?
Best regards,
Sa…
Part Number: TLC5916 Reading a Datasheet is hard enough without having to stumble over vague or clumsy writing--case in point: Section 9.4 of the TLC5916/5917 datasheet uses the following language to describe how to switch from the "Normal Mode", to one…
Part Number: TLC5916 Other Parts Discussed in Thread: TLC5947 , TLC6C5816-Q1 Hi, I need an IC like the TLC5916 but to support 28V output. It is important that it is 4-Wires SPI (SDI CLK LE OE). Is there an IC with characteristics very similar to this but…