I did some more testing and realized that when I write to the GRPPWM Register whatever value I write there is applied as a percentage to the values that were written to the individual brightness registers PWM0 to PWM7 and that is the actual brightness…
Part Number: TLC59208F Other Parts Discussed in Thread: LP5009 , Hi team,
Please advise, About the LED driver TLC59208F, have we done relevant reliability tests, such as the definition of the life of the internal MOS switching times?
Or related test…
Part Number: TLC59208F Other Parts Discussed in Thread: TLC59116 Hello E2E,
Customer would like to request sample code for tlc59208f.
Below is thier challenge.
Their product ’ s software is Linux base and kernel version is 4.4.
They need following…
Part Number: TLC59208F Hello,
My customer have two questions about TLC59208F below.
1. When the power supply is turned on, the voltage of VDD drops from 3.3 V to 2.5 V, is there a problem with IC?
Voltage drop time is about 20 to 30 ns.
…
Part Number: TLC59208F Dear Team
We found inTLC59208F datasheet
There is a gap in the description of the LED all call I2C Bus address default value,
At 9.5.6 says default 1001 000
At 9.6.1.8 says default 1101 000
The following screenshot,
…
Part Number: TLC59208F Hi Team,
Can you please help me understand if a 3V supply with +/- 5% tolerance over temperature range (hence min. 2.85V) is acceptable or if it has to be at least 3Vmin? Thank you!
Regards
Andreas
Part Number: TLC59208F Hi Team
My customer wonders will TLC59208F become timeout when wait time happens during transmit and receive?
If yes, how TLC59208F will work before and during timeout period?
Please let me know where it is described if this…
Part Number: TLC59208F Hi, As given in the reference manual to obtain a global blinking period of 1000 milli seconds the GRPFREQ – Group Frequency Register has to be filled with the value 23.
But with the value 23 the global blinking period achieved…