Part Number: TLC5922 Dear Texas Instruments Support,
I have a question regarding the correct procedure to enable the dot-correction (DC) function on the TLC5922.
To use the DC function properly, is it required to configure the On/Off register beforehand…
Part Number: TLC5922 Dear TI Support Team,
I am using two TLC5922 devices connected in a daisy-chain configuration to control LED brightness. All channels are set to the same brightness level, and all LEDs are operating under identical conditions. …
Part Number: TLC5922 Other Parts Discussed in Thread: LM3150 , TLC59116 Tool/software: Hi, TI expert.
I have a question about max current per channel of TLC5922.
According to the datasheet, Imax is confirmed to be 80mA for 16CH (OUT0~OUT15).
Q1…
Part Number: TLC5922 Tool/software: I have to drive the TLC5922 with a 30MHz SCLK @ Vcc=3.3V from a driver with VOH=2.2V and VOL=630mV. This is below the TLC5922 requirement of VIH>0.8*3.3=2.64V and VIL<0.2x3.3=660mV. It should be possible to use a level…
Part Number: TLC5922 Hi, expert:
We met TLC5922 ESD issue when test system ESD, and found some output has abnormal and hope to modify, I want to consult which pins are susceptible to ESD and are there some ESD protection recommendations for us? Thanks…
Other Parts Discussed in Thread: LM3150 , TLC5922
Tool/software:
Hi, TI expert.
I want to configure a circuit with the following specifications using LM3150. - Vin = 24V - Vout = 5V - Imax = 10A
Is there any application schematics that can be…
Part Number: TLC5922 Hi Team,
Customer is evaluating our TLC5922 LED driver, they found when the LED output is disabled with 0 current setting, the LED still slightly lights on with some leakage current. Do you have any suggestion to optimize it?
…
Part Number: TLC5922 Dear Specialists,
My customer is considering TLC5922DAP and has a question.
I would be grateful if you could advise.
---
Could you please let us know the operating junction temperature range and absolute maximum operating…
Part Number: TLC5922 Dear Specialists,
My customer is considering TLC5922 and has a question.
I would be grateful if you could advise.
---Question
Could you provide ideas and formulas for calculating the power consumption.
I couldn't find any…
Part Number: TLC5922 Other Parts Discussed in Thread: LP5861 , LP5018 Dear Specialists,
My customer is considering TLC5922 and has a question.
I would be grateful if you could advise.
---
Could you please let us know thermal resistance regarding…