Part Number: TLC5925 Good morning,
as written in thread title, I'd like to have a document which speaks about marking code of this component.
I don't found anything in the datasheet about manufacturing plant and above all data code.
I found only…
Part Number: TLC5925
Hi all. I have two questions. 1.How much is the maximum output cuttent at Vo>0.6V. Is it 45mA? 2.There is output current - output voltage graph in the datasheet. I attached the following, The temperature of this graph is 25℃ I would like…
Other Parts Discussed in Thread: TLC5925 Hello guys,
My customer wants to tied together all of TLC5925 output terminal to increase output current.
Is this usage no problem?
Your reply would be appreciated.
Thank you and best regards,
Kazuya Nakai.
Other Parts Discussed in Thread: TLC5925 Hello,
I have a problem with a board tha uses 2 TLC5925 cascaded.
Once I program a Word inside the components, LEDs that should stay ON start Flickering.
I'm pretty shure this defect not to be Hardware responsibility…
Other Parts Discussed in Thread: MSP430G2553 , TLC5925 Hi all,
I am cascading 9xTLC5925 chips by connecting the SDO of IC1 to SDI of IC2 and so on.
I am confused as to how I must send data from the controller MSP430G2553's SPI ?
Say I want to blink…
Other Parts Discussed in Thread: TLC5925 Hello,
I'am using an array of TLC5925 and a SPI Flash Memory on one SPI Port ( Arduino DUE ).
To write data on the Flash Memory I run the SPI with 84Mhz and give a SlaveSelect pin high to the memory.
The LED…
Other Parts Discussed in Thread: TLC5925 , TLC5926 Hi,
I have an evolution of the order of LED, but not the drivers. Those were configured to deliver ( with 2 drivers) 15mA and 50mA. Now , I have to use a transistor, and the current consumption will be some…
Other Parts Discussed in Thread: TLC5925 , TLC59281 Hello All,
Does anybody know what is the minimum output voltage( low saturation voltage) for TLC5925/59025 at currents 20mA?
Unfortunately for these IC there is no any information about output current…
Other Parts Discussed in Thread: TLC5925
Hello
I've got the this
Problem:
I use the TLC5925.
I don't know how the
controll the Outputs OUT0 - OUT15 done by SDI.
The Timing Diagram
and Truth Table in the Datasheet…
Other Parts Discussed in Thread: TLC5925 , TLC5927 , TLC5926 I want to use five of the TLC5925 together. My Problem: I
want, that all the Output-Channels of alle the 5 IC's make the same
Output Curent, which I want to dynamicale change between 5 to 45…