Part Number: TLC5927-Q1 Hi team
I checked the status of detection and operation when over temperature in datasheet as the below .
Are Tj.trip and Tsd the same?
The maximum value of Tj is displayed at 150°C.
Is there a problem if Tj.trip exceeds this…
Part Number: TLC5927 Hi
I am using constant sink LED driver for my application TLC5927 for LED display board. In my project it will be the main role. I have an issue. In hardware side one output pin of TLC5927 they have connected four LED's of cathode…
Part Number: TLC5927 Hi,
The control input pin seem to have Schmitt-Trigger Input but there is no information of hysteresis in Electrical Characteristics. Can you please check it internally?
Best Regard,
Satoshi / Japan Disty
Part Number: TLC5927 Hello guys,
One of our customers is going to evaluate TLC5927. The customer has some questions as the follows.
Could you please tell me your answer for the customer?
Q1. When LED anode voltage is powered up rapidly after TLC5927 OUTn…
Part Number: TLC5927 Dear TI,
I am using now your TLC5927 Driver but for new project I have to drive 400 LEDs and PCB need to be small. Can you please recommend an IC Driver with more than 16-channels,around 50mA pro channel, with SPI Interface and small…
Part Number: TLC5927 Hi,
Please let me know if TLC5927 can be used with Cascading Implementation. I believe that it can be used but I'm asking it because there is no Cascading Implementation of Schematic though it's in TLC592x-Q1 datasheet.
Best…
Part Number: TLC5926 Other Parts Discussed in Thread: TLC5927 , Hello Team,
Can TLC5927 be substituted for the TLC5926 without any board changes or software changes? Is the only difference the addition of short circuit detection? Does this change anything…
Part Number: TLC5927 Tool/software: TI C/C++ Compiler Hello All,
We are working on TLC5927 driver for drive multiple Seven Segment.
i send data to TLC5927 and it latch data on seven segment and it will display it.
But every 17 sec it will send 1 byte…
Part Number: TLC5927 Hello,
I have a design which I am using a pair of TLC5927 drivers. I am driving 32 Cree XLMLB LEDs, @ 40mA max each. My first question is how much heatsinking will I need to provide via the PCB. I am using 2 0Z copper on the board…
Part Number: TLC5927 Other Parts Discussed in Thread: TLC59116 Hi all Would you mind if we ask TLC5927? Is it possible to control each LEDs of brightness at individual port. Should we use TLC59116 instead of TLC5927? Kind regards, Hirotaka Matsumoto