Part Number: TLC59282
Hi team,
I am using the TLC59282DBQ with RIREF = 3.3 kohm.
The connection conditions for each output channel are as follows:
LED supply voltage: 12 V
LED configuration: Two LEDs connected in series
LED forward voltage…
Part Number: TLC59282 Hi team,
My customer designed TLC59282DBQR in their system but currently there is shortage issue, so they are asking alternative solution to replace.
I saw there are some TLC5928xx solutions and would like to know which one is…
Part Number: TLC59282 Hello Guys,
Good day.
Looking at page 12 of the datasheet where it shows how to set up the resistor on IREF to ground. Our customer have a 50K resistor there to set the current at 1 mA, which is too low according to the recommendations…
Part Number: TLC59282 Hi
We are using TI led driver TLC59282 and we have some timing issues with serial data.
I’m trying to fix this issue but could you clear one thing.
Propagation delay SOUT is stated 8-20ns, but is not clear is it over temperature…
Part Number: TLC59282 Other Parts Discussed in Thread: LP5018 Can we directly connect Blank pin to ground?
We are using only one IC and controlling it through I2c.
Part Number: TLC59282 Hello,
I have a quick question about TLC59282.
OUT0 to OUT15 ins are for LED sink.
for example if I have below values:
Vdd = 5v
Vled = 5v
Iref = 20ma
Rext = 2.55K
LEDs forward voltage is 2.2v
Then do I need to add…
Part Number: TLC59282 Hi E2E, Good day.
The datasheet mentions that there are Schmitt trigger buffers on the inputs (clock, serial in, latch). The customer would like to know the Schmitt trigger levels on TLC59282 with 3.3V supply, is it the Vih and…
Part Number: TLC59282 Hi team,
my customer is designing TLC59282 and in their application, they wanted to disable the LED during power up, so they pull the BLANK pin high, before turning on the Vcc.
The series resistor Rs is 33 ohms. In our datasheet…
Part Number: TLC59282 Hi,
TLC59282 and other TLC59xx devices have no minimum Propagation delay from SCLK to SOUT but I think it should be specified because there is possibility of concern as below. Could you please give your opinion about this concern…
Part Number: TLC59282 Hi
Could you please help to inform me. I have question I want to know your product TLC59282 is same with JXI5020 (I have only Chinese version) product from Macroblock or not. because I find a spare part and found picture reference…