Part Number: TLC5940 I'm an newbie for tlc5940 . I got TLC5940 EVM from my boss. According to the datasheet,1 GS Data Output Cycle consists of 4096 pulses.
I got a sample and sample code of TLC5940 EVM( USBv0.7_sourceCode, MCU: TUSB3210,software :LED…
Part Number: TLC5940 Other Parts Discussed in Thread: TLC5944 , Hi team,
Can you answer the following customer question please?
Unfortunately, the data sheet of the TLC5940 does not provide very detailed information about the Power-ON behavior. For…
Part Number: TLC5940 Hi,
I have developped my board based on TLC5940 as you can in the joined picture.
I have cascaded 15 of this IC. having finishe the development I order the board and start doing some Test. It happen out of the 10 board that I…
Part Number: TLC5940 Hi!
The TLC5940 is power by a 5V domain for VCC and the BLANK signal have a pull-up to 5V.
To prevent random channel turn-on, BLANK should be pulled high firstly. For this reason I have a pull-up to the 5V.
The LED:s are powered…
Hi Roeland,
I'd like to answer any application issues of TLC5940, but your question is more relate to the STM32 IDE. I think you need to contact ST company for help.
Sorry we have no Python library for TLC5940. These may not come from TI.
I will suggest to refer the below link for programming, www.ti.com/.../slvc106.pdf
Regards,
Shawn.
Part Number: TLC5940 Dear all,
I need a LED array design which need 300mA current each channel, but TLC5940 can provide 120mA each channel max. Can I paralleled TLC5940 outputs to provide High-Current outputs for my design ?
Any help will be appreciated…
Hello Kenneth
Sorry I found the answer yesterday and I didn't post immediately here.
Yes I sent the BLANK at the right time.
The problem was that the output pins of the Raspberry Pi 3 are either giving 0V or 3.3V and I supplied power to the TLC5940…
Part Number: TLC5940 Hi team,
I have a question for maximum cascaded devices.
I understand that the maximum number of cascaded devices is 40.
For example, if the clock speed is quite low, will the maximum number change?
Is it a maximum of 40…
Part Number: TLC5940 Hi team,
I have some questions about the absolute maximum rating of the output current.
It is written that Output current is DC 130mA.
Does this mean that it does not include instantaneous current such as power supply transient…