Part Number: TLC59581 Hi Team,
It was said in the forum that in order to achieve a required frame rate, you can reduce the number of sub periods by reducing the PWM resolution.
However, the method of configuring the number of PWM bits to a value between…
Part Number: TLC59581 Tool/software: 코드 컴포저 스튜디오 Set with FC DATA (MAXLINE 15) Controlling 16 LED lines GS BANK Setting well.
GS BANK line Counter 1. When GSCLK is in operation, lines 0~31 are executed? 2. When GSCLK is operated, is the 0~15 line executed…
Part Number: TLC59581 For Writing FC1 and FC2, as per datasheet and FC1 and FC2 Issues in forum stated that generate the LAT signal along with SCLK signal.
My Question is:
For SPI Clocks (SCLK) through SPI data writing in SPI mode, how we can write the…
Part Number: TLC59581 Hi,
FC2 offers an impressive number of display enhancement possibilities. Unfortunately, not all FC2 bits are clearly documented.
For example, what is the purpose of Reverse_V _G field (bits 38, 39)? They "control reverse voltage…
Part Number: TLC59581
Hi,
I have two TLC59581 chips in daisy chain configuration. Clock and data signals are formed with FPGA. SCLK frequency is 2MHz, GCLK is 4MHz, data on SIN line is set up 150ns before SCLK rising front.
I can shift GS data into memory…
Part Number: TLC59581 Hello team,
The customer is evaluating TLC59581. However he do not know how he adjust the timing among WRTFC, SCLK and LAT. He is using 3 pcs of TLC59581 such as the following excel file. /cfs-file/__key/communityserver-discussions…
Part Number: TLC59581 I have been reading out the default (on power up) values for the FC1 and FC2 registers and while most of the fields match what is documented in SLVA744.PDF, there are two fields in FC1 that don't. These fields are LODVTH and…
Part Number: TLC59581 Other Parts Discussed in Thread: TLC59582 , TLC5957 , TLC5958 , TLC6946 , TLC59283 Team,
1) Do we have some guidelines/advises/examples to use TLC59582/TLC59581/TLC5957 for a BW (ie black and white) 8x32 Matrix?
-Can 1 single device…
Part Number: TLC59581 Hi Team,
Can I get your help with Serial commands for the TLC595xx devices?
1. The Serial/SPI commands for the TLC595xx series devices aren't very clear in the datasheet.
-Could you provide a register map and maybe some annotated…
Part Number: TLC59581 Hi Team,
My customer is trying to use the TLC59581 for a matrix display and running into concerns with GCLK, can you help verify a few things for me?
They are doing 8 scan lines and want to achieve 120 frames per second in the 8x8…