Part Number: TLC59711 I have 20 boards chained together and can't seem to get a faster refresh rates than 0.04 seconds. This is just using a simply python script:
import argparse
import board
import busio
import time
import modules . ada_tlc59711 …
Part Number: TLC59711 Other Parts Discussed in Thread: TLC5971 , Team,
TLC59711 and TLC5971 (HTSSOP-20) seems to be very close (same package, same pinout): www.ti.com/.../compare.html
I have found the below post but it does not give 100% the confidence that…
Part Number: TLC59711 Other Parts Discussed in Thread: TLC5948A Looking at the D/S for this device, I do not see any shutdown pin which I can use to have the device consume no current when not used.
Since our system is battery powered and will contain…
Part Number: TLC59711 Hello E2E Experts,
Good day.
A quick question: Say I got high current LEDs which I wish to control using this device, is there some way to bypass its maximum 60mA current per channel? For example, let the device control a FET and…
Part Number: TLC59711 Hi All,
I am trying to create a very smooth fade in/fade out process using this device but for some reason when entering very low numbers
into the PWM value of a given channel (say the values 1 and then 2 and then 3) I see relatively…
Part Number: TLC59711 Hello All,
A costumer was looking to use 30 TLC59711 units in cascade for an HMI interface.
The original design had VLED=Vcc=Vreg=3.3, after checking the used LED forward drop at 10mA, the supplier estimate the maximum value at 3…
Part Number: TLC59711 Hello, We are testing the TLC59711 for our applications but we are experiencing some problems. For now, we only have 2 RGB LEDs connected to Out0 and Out3 and if we try to turn on the other outputs the LEDs start to flickering. We have…
Part Number: TLC59711 Hey,
I am looking to have VCC/VREG run at 5 V and VLED run at 3.3V through one 2.9V LED. Will this be enough voltage headroom to operate?
Thanks, Jacob
Part Number: TLC59711
In this manual,
on page 20, there's a section called 224-bit shift register that describes the shift register as 224 bits wide but in the next section it mentions a 244 bit shift register. Which one is correct?
Part Number: TLC59711 Hello, I am trying to drive a brushless DC motor with an APF27 but I do not have enough PWM output. Therefore, I tried to use the TLC59711. I used exactly the same design as the one presented in the datasheet (with a 3.3 kOhm resistor…