Part Number: TLC59731 Hello Team,
SDI data transfer rate is specified with 20kHz minimum. Why this limitation, please?
What if my frequency will be as low as 5Hz?
Thanks and Best Regards,
Hans
Part Number: TLC59731 Other Parts Discussed in Thread: TLC5973 Hello,
I just need a simple code example to get one single TLC59731 going.
As I understand I just need to send for bytes via SPI:
void set_rgb_led(signed int8 red, signed int8 green, signed…
Ok, did eventually manage to get this going. It really is the datasheet at fault here. Perhaps the most ambiguous and incomplete datasheet TI has ever produced?
It would appear that the Tcycle measurement sequence is the time between the first rising…
Other Parts Discussed in Thread: TLC59731 Hello,
I am looking for convenient ways to configure/program outputs of TLC59731 for testing purposes after building several prototypes in our lab. Wonder if TI has something like a demo board that could do so…
Hi Lidong,
Recommend connecting adjacent pins (connection 1 as you mentioned) to reduce trace length and therefore improve stability when paralleling multiple outputs.
We only have TLC5973 / TLC59731 that implements a single-wire interface.
Best Regards…
Other Parts Discussed in Thread: TLC59731 Dear team,
a customer of mine is interested in the TLC59731. He would need more information about the protocol (single wire interface).
Do you have some app notes or user guides?
Also, could you please give more…
Other Parts Discussed in Thread: TLC59731 Hi~ There~
I got a question on TLC59731 t cycle measurement sequence from my customer as below.
There is a different phrase at 8.4.2.1 and 8.5.1.1.
Would you please let me know whether this is mis-typo or there…
Other Parts Discussed in Thread: TLC59731 Hello, Currently I have an Arduino Uno outputting 0-5V pulse signals to program my lighting devices via a TI protocol call Single-Wire communication for TLC59731. Since there are so many lighting devices (800 of…
Other Parts Discussed in Thread: TLC59731 Hello,
I am wondering what is the current shape of the input pulse signal looks like on TLC59731?
I am aware that the voltage signal input shape is pulse signal between 0 and ~5V, but not sure what the current…
Other Parts Discussed in Thread: TLC59731 Hello,
I am currently working on TLC59731 and this is also my first time dealing with EasySet so please bear with me here as I have some problems writing output on Out#3 while Out#1 and Out2 have no problem.
Long…