Part Number: TLC6983 1. How is the internal GCLK generated? Is it a PLL multiplier from the external SCLK? Or is there an internal osc? I had access to the EVM header configuration worksheet, but it has a rule for GCLK to be between 40MHz to 160MHz and…
Part Number: TLC6983 Other Parts Discussed in Thread: TLC6984 Tool/software: Hi Expert,
Our customer wants to use TLC6983 for Transparent LED Display.
Their specification is 1080x1920 (RGB) resolution.
How many TLC6983's are required to support…
Part Number: TLC6983 Tool/software: LED Driver group,
Our customer would like to run the SCLK for TLC6983 at 40 kHz. Is there a minimum clock spec?
Do you have any concerns with them running 128 RGB LEDs at such a low frequency?
Thanks, Darren
Part Number: TLC6983 Other Parts Discussed in Thread: TLC6984 , , LP5891 , LP5890 For TLC6983, TLC6984, LP5890, LP5891, the SCLK Timing Requirements are as follows:
TLC6983, TLC6984:
f.cycle.max = 25 [Mhz] --> T.cycle.min = 40 [ns]
T.high.min = 18…
Part Number: TLC6983 Tool/software: Can you please point out what is the right peripheral to be used to drive the LED display controller?
I've not been able to find the right interface either on MCU or CPU.
The EVM seems to use an MSP430 with an emulated…
Hello, I would like to create a LED matrix for a product. The specifications are
a 16 x 16 matrix
that is monochromatic
but with the corners of the matrix cut off to fit on a round PCB
controlled by a STM32 MCU
I read that the CCSI interface…
Part Number: TLC6983 When a short occurs for each color in a product designed with 30 SCAN, 30 LEDs light up like GREEN + BLUE. In this case, it is difficult to find which LED has the short circuit. I am looking for defects by removing the LEDs one by…
Part Number: TLC6983 Other Parts Discussed in Thread: LP5890 , LP5891 , TLC6984 , MSP430F5529 I hope to get the sample code of 2 devices of TLC6983 for LED 32x32xRGB 3 page RGB color screen display reflash 60Hz.
I will use a MPU of 120MHz 32 bit ARM…
Part Number: TLC6983 Hi, Project requirements: 1. LED matrix driving (NO RGB,all same color LED) 2. VCC-3.3V 3. SPI Interface in daisy chain 4. LED current- 40mA 5. LED Open/short detection 6. PWM dimming 7. Auto scanning I checked TLC6983 IC datasheet…