Part Number: TLC6C5912-Q1 Hello,
In the below E2E thread, 1nF caps are recommended for DRAINx pins:
What is the maximum capacitance which could be inserted? e.g., can we put 100nF caps instead?
Best, Masaru
Part Number: TLC6C5912 Hi team,
My customer considers to use TLC6C5912 and its LED current will be 2mA.
[Question]
Is there limitation for minimum drain current?
[Background]
I think there would be no limitation for minimum drain current, but datasheet…
Part Number: TLC6C5816-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 , , TLC6C598-Q1 , TPIC6C596 Hi
The customer wants to use cascade TLC6C5816-Q1 + TLC6C5912-Q1.
Is it possible to Serial Interface cascade like the picture below?
The following characteristics…
Part Number: TLC6C5912-Q1 Hi TI-team
Is it safe to use the Vcc and VI voltage settings with the following settings ?
1: VI(Logic input-voltage) is higher than Vcc(Logic supply voltage)
e.g:VI=5.0V, Vcc=3.0V
2:Apply voltage to VI(logic input-voltage…
Part Number: TLC6C5912-Q1 Hello E2E,
I have a customer who is implementing the TLC6C5912Q1 in the following way:
They have a pullup to 12V on the open drain outputs, with switching FETs between the output pins and the LEDs
Due to this, the output pi…
Part Number: TLC6C5912-Q1
Hi all,
Can you tell me the drain-to-source parasitic capacitance of output FET when the FET is off or the TLC6C5912-Q1 is disabled as below?
Thank you, RYO
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C5912 , TLC6C5816-Q1 On the product page for the TLC6C5912-Q1, an alternative part (TLC6C5816-Q1) is recommended for new designs. Does this mean that Texas Instruments is soon going to discontinue…
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C5712-Q1 Hello all,
Can you tell me the deglitch time for each fault detection functionality? Also, are these functions available when PWM duty is 100% or 0%?
Weak-LED-supply detection
Reference…
Part Number: TLC6C5912 RCK and SRCK transfer data to the storage register at the first rising edge or at the second rising edge ?Why does the actual test feel like the second rising edge transfer data to the storage register? My actual connection diagram is…
Part Number: TLC6C5912-Q1 Hello Expert,
Thank you for your special support everyday.
I have two question about TLC6C5912-Q1.
1,What is the maximum Rate current ?
2,When outputting in parallel, what is the maximum current value that can be passed to pin…