Part Number: TLC6C5816-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 , , TLC6C598-Q1 , TPIC6C596 Hi
The customer wants to use cascade TLC6C5816-Q1 + TLC6C5912-Q1.
Is it possible to Serial Interface cascade like the picture below?
The following characteristics…
Part Number: TLC6C5912-Q1 Hi TI-team
Is it safe to use the Vcc and VI voltage settings with the following settings ?
1: VI(Logic input-voltage) is higher than Vcc(Logic supply voltage)
e.g:VI=5.0V, Vcc=3.0V
2:Apply voltage to VI(logic input-voltage…
Part Number: TLC6C5912-Q1 Hello E2E,
I have a customer who is implementing the TLC6C5912Q1 in the following way:
They have a pullup to 12V on the open drain outputs, with switching FETs between the output pins and the LEDs
Due to this, the output pi…
Part Number: TLC6C5912-Q1
Hi all,
Can you tell me the drain-to-source parasitic capacitance of output FET when the FET is off or the TLC6C5912-Q1 is disabled as below?
Thank you, RYO
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C5912 , TLC6C5816-Q1 On the product page for the TLC6C5912-Q1, an alternative part (TLC6C5816-Q1) is recommended for new designs. Does this mean that Texas Instruments is soon going to discontinue…
Part Number: TLC6C5816-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 , Dear Support team
About TLC6C5816-Q1, TLC6C5912-Q1 Could you provide internal circuit of each pin? My customer want to check internal pull-up, pull-down and clamp diodes.
Regards
…
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C5712-Q1 Hello all,
Can you tell me the deglitch time for each fault detection functionality? Also, are these functions available when PWM duty is 100% or 0%?
Weak-LED-supply detection
Reference…
Part Number: TLC6C5816-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 ,
Dear Support team
Please let me know how to determine the value of input capacitor to be connected to VCC and how to confirm the actual board.
Part: TLC6C5816-Q1,TLC6C5912-Q1
R…
Part Number: TLC6C5912-Q1 Hello Expert,
Thank you for your special support everyday.
I have two question about TLC6C5912-Q1.
1,What is the maximum Rate current ?
2,When outputting in parallel, what is the maximum current value that can be passed to pin…
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C598 Hello all,
I would like to know if there are any pins pulled up or down internally in TLC6C5912-Q1. If so, can you tell me the resistances?
Regards, RYO