Part Number: TLC6C598 Hi,
We got a question from the customer about TLC6C598. Could you help us?
[Question] What is the recommended terminal proccecing for unused DRAINx pin?
Best Regards, tateo
Part Number: TLC6C598 Hello,
Do you think PWM dimming can be implemented by inputting PWM signal to G pin?
It looks feasible if the response is fast enough.
Thanks.
Regards,
Oguri (TIJ automotive FAE)
Part Number: TLC6C598-Q1 Other Parts Discussed in Thread: TPIC2810 , TLC6C5816-Q1 Hi team,
One of my Automotive customers require an LED Driver (Tell-Tale LED's) to drive 6 LED's. They require the driver to have I2C interface capability.
I have…
Part Number: TLC6C598-Q1 Dears
Customer's product is dashboard, some return equipment appear 8channels LED can't been turn on, After test and X-ray display customer found pin7(CLR pin) inner lead has been breaked ,pin7 is powered by VCC(5V) driectly…
Part Number: TLC6C598-Q1 Hi,
Let me confirm about below.
--
"When data is high, the DMOS transistor outputs are capable of sinking current. This pin also can be used for global PWM dimming."
According to datasheet there is above description…
Part Number: TLC6C598-Q1 Other Parts Discussed in Thread: TLC6C598 Any difference between TLC6C598 C QDRQ1 and the EOL TLC6C598QDRQ1? TLC6C598QDRQ1 can be replaced by TLC6C598 C QDRQ1?
Part Number: TLC6C598 Team,
I didn't see a recommended total current capability for this device. Is it safe to assume the device can handle 50mA*8ch = 400mA provided the thermal dissipation/junction temperature requirements of the package are met…
Part Number: TLC6C598
Hello
My customer is using TLC6C598 and they have EMI testing of pilot run product now.
We know TLC6C598 has slow tr/tf of drain output , but would you please let me know the
worst value of rise time/ fall time of RCK,SRCK and SER…
Part Number: TLC6C598 Other Parts Discussed in Thread: TPIC6C596 , I started off with a TPIC6C596, which in turn is a ULN2803 with a serial interface on the front end, using it to drive 8 relays (24V @ 17mA each)
The TPIC6C596 has a problem in that it won…