Hi Youhei,
1. About your question, do you want to know the following information?
Time1--> The time from power-on to input CLR logic low.
Time2--> The time from input CLR logic high to OUT active?
For the Time1, we haven't focused on minimum time…
Other Parts Discussed in Thread: TLC6C598 , TPIC6B596 Hi support members,
Datasheet shows 50mA for drain current.
But pulse drain current can be estimated as following thread.
Is 60mA pulse current acceptable as absolue value with thermal care?
Regards,…
Other Parts Discussed in Thread: TLC6C598-Q1 Dear, Sir.
My customer is asking related to Thermal Shutdown Protection(TSD) function of
TLC6C598-Q1 as below. Please give your advice because it is not sure
on the datasheet.
1. Once TSD is activated, All channel…
Other Parts Discussed in Thread: TLC6C598-Q1 , TLC6C5912-Q1 , TLC6C598 Hello,
Please tell me Dissipation ratings of TLC6C598-Q1 and TLC6C5912-Q1. This product package is 20pin TSSOP. Could you also provide graph in conjunction with the above?
Best regards…
Other Parts Discussed in Thread: TLC6C598-Q1 Dear, Sir.
I know the internal circuit is a kind of confidential and this question is a type of such.
My customer would like to know the chip design is well considering on fail-safe-wise point of view.
The…
Other Parts Discussed in Thread: TLC6C598 Hi,
Are there any limitations, or recommmendations, regarding input transition rise/fall time for the power logit shift register TLC6C598?
Regards,
Per
I would like to confirm the supply(consumption) current.
In the datasheet, supply current is;
0.1uA typ., 1uA max. (All outputs off) @Vcc 5V and Tc=25degreeC
88uA typ., 160uA max. (All outputs on) @Vcc 5V and Tc=25degreeC
In this case how much is the…
Other Parts Discussed in Thread: TLC6C598-Q1 I would like to confirm the leak current of FET's for TLC6C598-Q1.
The condition is;
Vcc=0V, Drain voltage=12V, temperature range -40 to 95 degreeC (This IC is off and the battery connects drains of TLC6C598…
Part Number: TLC6C5816-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 , , TLC6C598-Q1 , TPIC6C596 Hi
The customer wants to use cascade TLC6C5816-Q1 + TLC6C5912-Q1.
Is it possible to Serial Interface cascade like the picture below?
The following characteristics…