Hi,tony
I'm working on a project about the driver of stepper motor.
I use also the TLC7524, and i connected the circuit as what Rafael proposed, my Vdd is 5V,Vref 5V.
But the maximum of the output is 4.4V, it can never arriver at 5V.
I don't know…
Other Parts Discussed in Thread: TLC2274 , TLC7524 I'm building a device to generate a sine wave. I have been working from the data sheet, and thus far haven't had any problems using the chip as a unipolar device. However, I can't seem to ge the bipolar…
Other Parts Discussed in Thread: DAC0800 , DAC0808 , DAC0802 , TLC7524 , TLC7528 , TLC7628 , TLC7225 , TLC7226 I am looking for a recommendation on a pair of ADC&DAC (not necessarily in one package together) to go with a Z180 CPU (Z80 or 8080 MPU compatible…
Other Parts Discussed in Thread: TLC7524 , OPA2237 Dear sir,
I am using TLC7524, SMD IC as DAC. VDD = 5V,Vref = 5V. The output of DAC i have given to OPA2237 ic,which is having +/- 15V supply.
I am able to see my data correctly on data lines, chip select…
Other Parts Discussed in Thread: DAC8581 , DAC8806 , DAC8801 , TLC7524 Hi,
I'd like to make a simple ECG simulator and my initial idea is to use precision bipolar DACs. The output is needed to be in the -2mV...+2mV range and with low noise to articulate…
Other Parts Discussed in Thread: VCA824 , THS3091 , THS6204 , PGA870 , TLC7524 , TL074 , TINA-TI , LMH6523 Hello,
I need to implement a variable voltage output amplifier....digitally controlled output voltage is ideal
the output needs to be a square wave of…