Part Number: TLC77-EP Hi Team,
Our customer would like to clarify about the high level output current of TLC77-EP. According to our customer,
Electrical characteristics table in the current datasheet revision for Output Voltage (high and low) specify…
Part Number: TLC77 Hi team,
Does TLC7733 have recommended range for Ct value? If so, could you tell me that range to share with the customer?
Best regards,
Takeshi Sasaki
Part Number: TLC77 Dear Specialists,
My customer is considering TLC7733 and has a question.
We would be grateful if you could advise.
---
TLC7733 is a supervisor for 3.3V.
However, datasheet P.6 of electrical characteristics( VIT-) describes 2.93mVtyp…
Part Number: TLC77 Dear Team,
Regarding the TLC7733IDR , the following is the circuit we designed. Is C173, C178, C177 required? In the case of R296 and C173, it should be for the design of the Push button, but in our design the input to the reset IC is…
Part Number: TLC77 Hi Team, We have a customer requesting for the Max Junction Temperature information of TLC7733IDR. If you have available information, kindly let me know so I can share it with our customer. Thanks! Jonathan
Hello,
As a long term strategy, I do recommend moving to a newer generation device. At this point we do not have any information on longer term plans for TLC7705MJG.
Here is another E2E post that could help with your design:
[FAQ] TLC77: Looking for newer…
Hello
I'm Not Found the Negative-going input threshold voltage and Min Value of Delay time for TA = -55°C to 125°C(TLC7701) at datasheet.
Please Can you tell me the this ELECTRICAL CHARACTERISTICS?
and Is V62/04604-04XE rating the Military…