Part Number: TLE2426
Tool/software: TINA-TI or Spice Models
Hi,
I have been working with Tina-Ti to create a design for an inverting opAmp circuit using an OPA350 or equivalent as a voltage follower whose input comes from a INA121, and which runs off…
Part Number: TLV8801 Other Parts Discussed in Thread: TLE2426 , , TLV6001 , LMV321 , TLV9062 , TLV9051 , TLV9052
Hi
I am trying to design rail splitter similar to TLE2426 since we are not able to use this part to package and availability limit. I am doing something…
Other Parts Discussed in Thread: TLE2426 Hi,
We are currently building an amplifier which must work across a wide range of temperatures, ideally up to 200°.
We would like to use the TLE2426 or something similar to generate a split rail supply from…
Other Parts Discussed in Thread: TLE2426 , OPA2192 , BUF634 Hi All,
I require a chip equivalent to TLE2426 with a higher current source/sink capability. The TLE2426 has 20mA source and sink capability.
Could you suggest me for 30mA current requirement? …
Other Parts Discussed in Thread: TLE2426 Hi from a 3 day old user. I seem to be getting some odd behavior from the TLE2426 model. All it does is output half the input voltage, but transient analysis seems to get it wrong. Or just maybe it's me? Circuit…
Other Parts Discussed in Thread: TLE2426 I am using a TLE2426 to create a virtual ground and need to know how much capacitance I can put on the output pin 1 or if you have any other suggestions to quench noise (100mv) on pin 1. it is being powered by a…
Other Parts Discussed in Thread: TLE2426 , MC33063A , LM337 , LM317 , TL082 Hi all
I am having a single side supply of +15 v and i would like to obtain +7.5V and -7.5 V from this supply. As I was going through the datasheet of TLE2426 I came to know that …
Hello Wade,
Sorry for the abhorrently late reply. As it turn out I wasn't setting up the agilent power supply correctly but I thank you for your responses.
Other Parts Discussed in Thread: TLE2426 , REF3030 My customer use TLE2426 in a DAQ board. the input votlage is 3V, which is below recommended 4V. the engineer want to know what is the potential risk. BTW, 3V is generated with REF3030
- i guess the output…
Other Parts Discussed in Thread: TLE2426 , OPA134 Continuing from my recent post: To eliminate noise and distortion in my audio circuit, I am convinced the solution boils down to two things, head room and ground current. I am extremely leary of audio noise…