Part Number: TLE4275-Q1 Other Parts Discussed in Thread: TL720M05-Q1 , Hi,
I need simulation model of below mentioned IC.
TLE4275-Q1 5-V Low-Dropout Voltage Regulator datasheet (Rev. I)
Please Sent me the Simulation model As soon as possible.
Regards…
Part Number: TLE4275-Q1 Other Parts Discussed in Thread: TLV62065 ,
Dear team,
our customer test the Iout before the Cout , when power on, the Iout have 600mA overshoot with 22uf Cout and 800mA overshoot with 220uf Cout.
First, we want to know is this…
Part Number: TLE4275-Q1 Other Parts Discussed in Thread: TPS7B67-Q1 Team,
Do we have a pin compatible alternative to our TLE4275QPWPRQ1?
My customer is running into availability issues, that near term we are not able to address.
Thanks
Viktorija
Part Number: TLE4275-Q1 Hi Engineer,
I would like to check if TLE4275-Q1 is AECQ100 qualified?
I only see that mentioned on ESD spec in datasheet, but not on the first page.
please help, thanks.
Part Number: TLE4275-Q1 Dear, Sir.
I would like to double-confirm about simple matter as below.
Please give your advice.
I wonder all NC pins on 20HTSSOP can be connected to GND & thermal pad zone
to expand the exposed Cu area for heat-sink?
…
Part Number: TLE4275-Q1 Dear Sir or Madam:
My customer need the "Positive input transient " parameter of TLE4275QKTTRQ1, like below picture:
Can you help?
Thanks!
Part Number: TLE4275-Q1 I am using the TLE4275QKTTRQ1 on a product and it states that it is "Reverse-Polarity Proof" but we are seeing catastrophic failure at 85°C and -30V. I am using a 1uF ceramic cap on the input (pin 1) and 33uF tantalum cap on the…
Part Number: TLE4275-Q1 Dear sir,
VCC=5V BATTERY=0V, The SCH is as below
Question: The vcc(5v) for download, we found the vcc fall when download which causes the downloading of the program to fail. We had replaced TLE4275 to Infineon‘TLE4275 and ON…
Hello,
The 5V rail of a power supply is not stable under a 100ma load... - Input to the regulator is 12-16V DC from the vehicle battery. We are also noticing a high frerquency audible hum from the regulator in normal operation. Any suggestiong/review of…