Part Number: TLIN1029A-Q1 Hi Team, Compared with 1021 and 1029, 1021 has two more pins, WAKE and INH. Considering the supply situation of the chip, customer have made a compatible design on the peripheral circuit of the chip so that the two chips can…
Part Number: TLIN1029-Q1 Hi Team
There is a good new that DIN TLIN1029Q1
1. I want to confirm with you, what is the maximum input current of TLIN1029Q1 under normal operation? I want to confirm the specifications of the LDO from my side
2, Please help…
Part Number: TLIN1029-Q1 Hi team,
Could you teach the difference of 'TIN1029DRBRQ1' and 'TLIN1029"M"DRBRQ1'?
What is the change point between non-M and M?
Best regards,
Part Number: TLIN1029-Q1
Hi team,
Does TLIN1029 have specification for input transition rise or fall rate ?
Are there any concern if slow signal is coming for input ?
Thank you and best regards,
Michiaki
Part Number: TLIN1029-Q1 Hi TI-team
My customer have a question about the "7.6 Electrical Characteristics over operating free-air temperature range (unless otherwise noted)" listed on page 6 of the datasheet.
Is this correct with the recognition…
Part Number: TLIN1029-Q1 Hi Team,
Is there a way to check if the Slave's Hardwire connection is OK on the LIN Master? -When Auto Addressing, you can check the Slave connection status of course, but the customer needs to check if the Hardwire connection…
Part Number: TLIN1029A-Q1 What is the difference between TLIN1029 and TLIN1029A?
I think TLIN1029 is an improvement of ERRATA and an improvement of ESD.
However, I noticed that the block diagrams of these two products are different. Why was "Dominant…
Part Number: TLIN1029-Q1 Hello team,
LIN standard specify the maximum length is 40m.
What is the limitation for specification of max length at 40m ?
And our device TLIN1029 is also max length 40m ? or can TLIN1029 be applied to longer length ?
Thank…
Part Number: TLIN1029-Q1 Hello team,
Could you give us the storage temperature and “recommended” operating ambient temperature ?
We understand the operating ambient temperature is described in absolute maximum ratings but let me confirm if…