Part Number: TLK10002 1、Whether it is feasible that IO of eight single chip simulate MII ?
2、if TLK10002 Can be controlled by eight single chip microcomputer?
Part Number: TLK10002 Hi,
I purchased the TLK10002EVM board and the computer has problem to recognize the USB device driver after I installed the GUI software successfully. Please share your experience in resolving this USB driver issue.
Thanks
Denni…
Hi Drew,
The customer found the TLK10002 on TI website.
This product seems to have a PRBS error count feature. Any reason for recommending the DS series instead of the TLK10002?
Thanks,
JH
Part Number: TCI6638K2K Dear Team,
My customer has a question on using TLK10002 to increase CPRI interface from 4.9Gbps to 9.8Gbps. please see their questions below:
Can we use TLK10002 to aggregate two AIF links of TCI6638K2K and obtain one 9.8 Gbps…
Part Number: DS100MB203 Other Parts Discussed in Thread: TLK10002 , TLK10232 Dear Sir/Ms.
I'm sorry to trouble you. I'm at home in SMPS not in Interface.
This project for 10G CPRI's media converter and needs the following functions:
1. 10G…
Part Number: TLK10002 For TLK10002 normal operation, we need to first apply an external clock to TLK10002's REFCLK0 to let CDR working probably and produce a good recovered clock,
then connect the recovered clock to an external dejitter IC lmkxxxxx…
Part Number: TLK10002 Other Parts Discussed in Thread: TLK10232 Hi team,
My customer wants to use TLK10002 in a 5.15625G=>10.3125GHz Ethernet application.
Does our chip support such data rate?
Do we have any similar application information to share…
Part Number: TLK10002 Other Parts Discussed in Thread: TLK10022 We are going to use the TLK1002 to perform the serialization / deserialization of the TMDS lines of an HDMI / DVI signal, b ut have a few questions :
1. The Clocking examples of the TLK10022…
Other Parts Discussed in Thread: TLK10002 , TLK10232 Hello colleagues,
Bit 3 of the Register HS_SERDES_CONTROL_2 (R3.3) is used to control the scrambled data capability of HS port. But I cannot find any more words about the scramble function. Can you give…